i.MX 8M Quad SMP multicore operation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Quad SMP multicore operation

787 Views
anhui527
Contributor III

Hi, I want to use i.MX 8M Quad with u-boot only, to run a task in SMP mode multicore? Which steps I should do to enable this mode? Which part of u-boot needs to be modified?#i.MX 8M Quad

0 Kudos
Reply
1 Reply

715 Views
igorpadykov
NXP Employee
NXP Employee

Hi An

I am afraid this is not supported in nxp uboot releases and may be posted on

uboot mail list U-Boot Info Page 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply