i.MX 8M QSPI boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,177件の閲覧回数
peter_gabor
Contributor I

Is it possible to boot from QSPI on NXP i.MX 8M EVK board MCIMX8M-EVK? Schematics file says "QSPI boot is not supported by ROM". If yes, what will be the Boot switch configuration? Regards Peter Gabor

ラベル(1)
0 件の賞賛
返信
1 解決策
1,170件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Peter

 

>Is it possible to boot from QSPI on NXP i.MX 8M EVK board MCIMX8M-EVK?

 

not, sorry, as described in sect.6.1 System Boot  i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual

The boot ROM supports these boot devices:
• NAND flash
• SD/MMC

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,171件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Peter

 

>Is it possible to boot from QSPI on NXP i.MX 8M EVK board MCIMX8M-EVK?

 

not, sorry, as described in sect.6.1 System Boot  i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual

The boot ROM supports these boot devices:
• NAND flash
• SD/MMC

 

Best regards
igor

0 件の賞賛
返信