i.MX 8M QSPI boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M QSPI boot

Jump to solution
614 Views
peter_gabor
Contributor I

Is it possible to boot from QSPI on NXP i.MX 8M EVK board MCIMX8M-EVK? Schematics file says "QSPI boot is not supported by ROM". If yes, what will be the Boot switch configuration? Regards Peter Gabor

Labels (1)
0 Kudos
Reply
1 Solution
607 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

 

>Is it possible to boot from QSPI on NXP i.MX 8M EVK board MCIMX8M-EVK?

 

not, sorry, as described in sect.6.1 System Boot  i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual

The boot ROM supports these boot devices:
• NAND flash
• SD/MMC

 

Best regards
igor

View solution in original post

0 Kudos
Reply
1 Reply
608 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

 

>Is it possible to boot from QSPI on NXP i.MX 8M EVK board MCIMX8M-EVK?

 

not, sorry, as described in sect.6.1 System Boot  i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual

The boot ROM supports these boot devices:
• NAND flash
• SD/MMC

 

Best regards
igor

0 Kudos
Reply