i.MX 8M Plus Yocto Image Bitbaking

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX 8M Plus Yocto Image Bitbaking

跳至解决方案
10,962 次查看
fozen
Contributor I

Hi,

I have i.MX 8M Plus EVK Board and I don't know anything about linux environment. I have started to read "i.MX Yocto Project User's Guide", "i.MX Linux® User's Guide" and "Freescale Yocto Project Tutorial" pdf files. I have a Ubuntu Machine (22.04) and sd card (32 GB) with sd card reader. I want to boot my EVK Board from sd card. I have started with "i.MX Yocto Project User's Guide" at first and I stuck bitbaking part of the document. After I write "$ bitbake imx-image-multimedia" command it starts bitbaking, I face with some errors. I don't know it is okay or not but I want to continue to processes. My sd card is empty and when I want to write "$ sudo dd if=<image name>.wic of=/dev/sdx bs=1M && sync" command I see that I need a wic extension document. I search it with find command but there is not any wic file.

I thougt that's reason is faults as I mentioned above. Could you help me to have wic file. I add fault's image. 

 

0 项奖励
回复
1 解答
10,946 次查看
edwardtyrrell
Senior Contributor I

Before worrying about how to put your image on the SD card, fix the issues first. If you don't fix the build you will have nothing to put on the card! In your photograph it shows the build failure, it fails to fetch certain packages. Make sure you have installed the host packages as describe here by QMiller https://community.nxp.com/t5/i-MX-Processors/IMX8-fatal-error-attr-xattr-h-No-such-file-or-directory... 

Also for your first time try using a smaller image, like a core-image-minimum or core-image-base (or imx-image-xxx depending on your document)

 

在原帖中查看解决方案

7 回复数
10,911 次查看
fozen
Contributor I

Hi, 

I have also updated and downloaded host packages except below. As I wrote before I use 22.04 Ubuntu version and it seems there is no package support for them.

E: Unable to locate package pylint3
E: Unable to locate package lz4c

E: Unable to locate package pzstd
E: Package 'python' has no installation candidate

I have pylint instead of pylint3. I could not load python

0 项奖励
回复
10,903 次查看
edwardtyrrell
Senior Contributor I

Hi,

This is getting a little out of the forum's point and more Ubuntu packaging issues; are you on a native machine or VM? Only thing I can suggest is you look at each error as an individual task and solve each one separately. It can take quite a while and lots of googling to crack such issues. If you're new to the Linux environment it can be quite challenging but we've all been there!

Here's a couple of links for the lz4c 

https://installati.one/ubuntu/20.04/lz4/ 

Locate package issues

https://askubuntu.com/questions/378558/unable-to-locate-package-while-trying-to-install-packages-wit...  

 

Also, you need to use/fix python3 packages where required.

 

Edit: The 31 March 2022 imx8 Yocto project user guides suggests 20.04 or later; I've been using Yocto for around 8 years for work on a number of devices and have found the later versions of Ubuntu (post document date) can give build headaches. A few times I've had to roll back my build machine version (imx7sabresd for example) to the one stated in the doc.     

 

Hope this helps..

 

 

 

 

 

0 项奖励
回复
10,935 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @fozen 

The first task to fetch source file is failed. Firstly You need to make sure that you can access to these links for source file to fetch based on your local network. 

As for the wic files to flash SD card. You will see it under this directory ./<your build directory>/tmp/deploy/images/../*.wic.bz2, If the whole build with success.

 

Best regards

Harvey

 

0 项奖励
回复
10,622 次查看
fozen
Contributor I

Hi @Harvey021 ,

There is an update on my side. I changed OS, now I use Ubuntu 20.04 LTS. I have not faced with package problem. There is a problem on just one task while bitbaking. I have tried many many times but linux-imx-5.15.32+gitAUTONIC+fa6c316859-r0 do_fetch task was never completed. What could be the reason ? Some guys say weak internet connection but I want to be sure on this topic. Is it possible to change 5.15.32 to different one ? I don't know if it works or not, I am just asking.

0 项奖励
回复
10,611 次查看
edwardtyrrell
Senior Contributor I

As a test you could try rolling back. In the doc you'll see the following repo set up: 

mkdir imx-yocto-bsp
cd imx-yocto-bsp
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-honister -m imx-5.15.5-.0.0.xml
repo sync

Change these options to select different flavours/kernels: -b imx-linux-honister  and  -m imx-5.15.5-.0.0.xml

In your attached image your kernel was 5.15, did you move away from that build? You could try that again on your new 20.04 machine. According to docs.yoctoproject there are a few kernel options (and one not listed in the removed list obviously). You don't have to specify the -m kernel option if you can't find any references to the xml file, it will just use the default.

  • linux-yocto: removed version 5.4 recipes (5.14 and 5.10 still provided)

 https://docs.yoctoproject.org/migration-guides/release-3.4.html 

 

10,442 次查看
fozen
Contributor I

I could do the process successfully. The problem was bad internet connection, I brought pc to home and bitbake process completed. I could place sd card image to sd card and now I can run iMX board via SD Card. Thanks a lot.

0 项奖励
回复
10,947 次查看
edwardtyrrell
Senior Contributor I

Before worrying about how to put your image on the SD card, fix the issues first. If you don't fix the build you will have nothing to put on the card! In your photograph it shows the build failure, it fails to fetch certain packages. Make sure you have installed the host packages as describe here by QMiller https://community.nxp.com/t5/i-MX-Processors/IMX8-fatal-error-attr-xattr-h-No-such-file-or-directory... 

Also for your first time try using a smaller image, like a core-image-minimum or core-image-base (or imx-image-xxx depending on your document)