i.MX 8M Plus - VPU / Video Decoding of custom resolution

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX 8M Plus - VPU / Video Decoding of custom resolution

1,472 次查看
sistdee
Contributor I

Hi,

I have a question regarding the i.MX 8M Plus and the VPU (Video Decoding).

Is it possible to connect the i.MX 8M Plus to a display with following specs:
Resolution: 2700*350
FPS: 60 FPS
Interface: 4 lanes MIPI-DSI

The video encoding format that will used is h.264.


According the specification, the 8M Plus VPU allows a max resolution of "1080p60" / 1920x1080@60FPS. Is it possible to use the VPU (Video Decoding) with a display with a wider but flatter resolution (2700x350)?


Thanks!

Regards,

Simon

0 项奖励
回复
3 回复数

1,450 次查看
sistdee
Contributor I

Hi Igor,

thanks for the fast reply!


What changes are neccessary to make the display work?

Is a change in the VPU or MIPI kernel driver needed or can all changes be done in the device tree configuration?

Regards,

Simon

0 项奖励
回复

1,442 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Simon

 

>What changes are neccessary to make the display work?

 

please create new thread as this is new question.

For new LCD there is no need for vpu changes.

 

Best regards
igor

0 项奖励
回复

1,465 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Simon

 

>Is it possible to connect the i.MX 8M Plus to a display with following specs:
>Resolution: 2700*350  FPS: 60 FPS

 

yes

 

> Is it possible to use the VPU (Video Decoding) with a display with a wider but flatter resolution (2700x350)?

 

yes

 

Best regards
igor

0 项奖励
回复