Hi! NXP Engineer
in my design, refer to NXP EVB(imx8m plus+LPDDR4+eMMC+RTL8211+TC358743+USB 2.0),
and only VPU is used, CPU volume is 20%,
but , when the hot stable state, SoC temperature rise is above 50℃, LPDDR4 is 46℃, eMMC is 40℃.
They are very high, and then how to calculate the power consumption of SoC/LPDDR4/eMMC .
For SoC/LPDDR4, the heatsink is neccessory?
Best Regards.
Best Regards.