i.MX 8M Plus | Power Consumption and Overheat

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Plus | Power Consumption and Overheat

3,105 Views
NeuralBlue
Contributor I

I'm currently measuring the power consumption of iMX 8M Plus and I noticed high power consumption & a lot of heat development.

How to replicate:
1) Install Yocto on the iMX 8M Plus SoM, following this document https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf 
2) Display, ethernet disconnected.
3) Boot up the system and measure current and voltage.

Results:
1) the board, powered at 5,00V consumes 0.340 A for a total of 1,7 W.
2) Consumption is stable over time. 
3) CPU 0.4% out of 400% stable.
4) Clock is at 1600 Mhz
5) Heatsink is untouchably hot,
6) Both thermal zones are at 48 to 53 degrees at room temperature.

Question
Clearly there should be a clever solution to this, but I first need to understand how to discriminate if is this a sw or hw problem. Any idea? 

Hint
I've found this: https://www.nxp.com/docs/en/application-note/AN12410.pdf relative to iMX 8M Mini but not the equivalent for iMX 8M Plus. Is it available?

0 Kudos
2 Replies

3,017 Views
NeuralBlue
Contributor I

Thank you Igor,

I hope that in future SW version idle power consumption will go down. Let's keep posted in this thread.

Is thermal throttling enabled?

Thank you

V.

0 Kudos

3,056 Views
igorpadykov
NXP Employee
NXP Employee

Hi Volta

 

>..solution to this, but I first need to understand how to discriminate if is this a sw or hw problem...

 

yes this may be software problem

 

>..AN12410.pdf relative to iMX 8M Mini but not the equivalent for iMX 8M Plus. Is it available?

 

such document can be obtained through local marketing office, as this processor is not

publicly released yet, as described in below link : "PREPRODUCTION" in red.

 

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

 

1.jpg

 

 

Best regards
igor

0 Kudos