i.MX 8M Plus - I2C3 and I2C5 enable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Plus - I2C3 and I2C5 enable

Jump to solution
676 Views
colinbroderick
Contributor III

Hello,

On the imx8mpevk, I2C busses 3 and 5 are the ones exposed on the expansion connectors. But they don't seem to be enabled in core-image-base. Running i2cdetect on those busses gives

Error: Could not open file `/dev/i2c-5' or `/dev/i2c/5' : No such file or directory

Are any extra steps required to enable them? Other I2C busses are working but as far as I can tell they are not accessible on the expansion connectors.

Thanks

Tags (4)
0 Kudos
1 Solution
672 Views
colinbroderick
Contributor III

It seems like the main expansion connector, labelled as I2C3 in the schematic, is actually I2C2 in the image. So problem solved. Just an off-by-one thing I guess.

View solution in original post

0 Kudos
1 Reply
673 Views
colinbroderick
Contributor III

It seems like the main expansion connector, labelled as I2C3 in the schematic, is actually I2C2 in the image. So problem solved. Just an off-by-one thing I guess.

0 Kudos