i.MX 8M Plus FlexCAN running while CPU cores suspended

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Plus FlexCAN running while CPU cores suspended

739 Views
matbus
Contributor II

On i.MX 8M Plus, can the FlexCAN be alive while the CPU cores are suspended? With
hardware filters we can then have the FlexCAN interrupt the CPU on
specific frames and deliver them. I mean have the CAN controller and CAN
tranceiver fully running at some power consumption cost?

0 Kudos
Reply
3 Replies

730 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mattias

 

for such case one can look at sect.11.8.2.1.1.4 Stop mode 

i.MX 8M Plus Applications Processor Reference Manual

 

Best regards
igor

723 Views
matbus
Contributor II

Hi Igor,

 

Thanks for the reply. However, the FlexCAN cannot wake up on a specific frame here as I understand or am I wrong? We need to wake up on a normal CAN frame.

0 Kudos
Reply

718 Views
igorpadykov
NXP Employee
NXP Employee

one can try to leave FlexCAN running in low power mode configuring its CCM_CCGR53,54 registers,

clock gate control is described in sect. 5.1.7.6 CCM Clock Gating Register (CCM_CCGRn)  i.MX 8M Plus Applications Processor Reference Manual

 

Best regards
igor

 

 

 

 

 

0 Kudos
Reply