i.MX 8M Plus DDR stress test without USB OTG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Plus DDR stress test without USB OTG

Jump to solution
1,005 Views
tetsuro-okuyama
Contributor V

I want to execute the DDR stress test via JTAG or u-boot.
The target SoC is i.MX8MPlus.
If you look at this page, it only describes the method using USB OTG.

Can I do the DDR stress test with JTAG or u-boot for 8MP?

Labels (1)
Tags (2)
0 Kudos
1 Solution
948 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tetsuro

 

unfortunately sources of test are not available, sorry.

 

Best regards
igor

View solution in original post

3 Replies
988 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tetsuro

 

>Can I do the DDR stress test with JTAG or u-boot for 8MP?

 

sorry such option is not supported.

 

Best regards
igor

953 Views
tetsuro-okuyama
Contributor V

Hi, @igorpadykov 
Please tell me one more thing.

Is the source code for this tool available?
If so, please tell me the address of the repository.


Best regards,

0 Kudos
949 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tetsuro

 

unfortunately sources of test are not available, sorry.

 

Best regards
igor