i.MX 8M Plus DDR ECC documentation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Plus DDR ECC documentation

Jump to solution
1,872 Views
fd
Contributor III

Hello,

I'm looking at the DDR inline ECC functionality of the i.MX 8M Plus SOC, however I was not able to find complete documentation in the reference manual.

The U-Boot code uses the following registers

```

#define DDRC_SARBASE0(X) (DDRC_IPS_BASE_ADDR(X) + 0xf04)
#define DDRC_SARSIZE0(X) (DDRC_IPS_BASE_ADDR(X) + 0xf08)
#define DDRC_SBRCTL(X) (DDRC_IPS_BASE_ADDR(X) + 0xf24)
#define DDRC_SBRSTAT(X) (DDRC_IPS_BASE_ADDR(X) + 0xf28)
#define DDRC_SBRWDATA0(X) (DDRC_IPS_BASE_ADDR(X) + 0xf2c)
#define DDRC_SBRWDATA1(X) (DDRC_IPS_BASE_ADDR(X) + 0xf30)
#define DDRC_PDCH(X) (DDRC_IPS_BASE_ADDR(X) + 0xf34)
#define DDRC_SBRSTART0(X) (DDRC_IPS_BASE_ADDR(X) + 0xf38)
#define DDRC_SBRRANGE0(X) (DDRC_IPS_BASE_ADDR(X) + 0xf40)

```

and they are used in the `ddrc_inline_ecc_scrub()` function.

The reference manual, with reference to the ECC testing functionality, in the register `ECCCFG1` mention `ECCPOISONADDR0/1`, but they are not defined anywhere.

 

Where can I find documentation for all those registers?

Where can I find additional documentation on the topic?

 

A similar question was asked months ago, https://community.nxp.com/t5/i-MX-Processors/inline-ECC-in-i-MX8M-Plus/m-p/1212335/highlight/true#M1... but it did not get an answer.

Thanks,

Francesco

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,850 Views
Yuri
NXP Employee
NXP Employee

@fd 
Hello,

   I've sent You some comments directly.

Regards,
Yuri.

View solution in original post

0 Kudos
Reply
1 Reply
1,851 Views
Yuri
NXP Employee
NXP Employee

@fd 
Hello,

   I've sent You some comments directly.

Regards,
Yuri.

0 Kudos
Reply