i.MX 8M Plus Configure Settle Parameters

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Plus Configure Settle Parameters

1,295 Views
sachin_patel
Contributor III

Hi,

I am currently integrating a MIPI CSI-2 solution into our custom hardware. I'm aware of the table in this post https://community.nxp.com/t5/i-MX-Processors/Explenation-for-HS-SETTLE-parameter-in-MIPI-CSI-D-PHY-r... for the HS_SETTLE and CLK_SETTLE parameters, but am unsure if the same is true for i.MX 8M Plus.

Thanks,

Sachin Patel

0 Kudos
6 Replies

159 Views
pgugiclr
Contributor I

Hi,

So where can I get those values for iMX8M Plus?

Are they the same as the table above?

Thank you

0 Kudos

1,188 Views
jeremie1
Contributor II

Hello @igorpadykov ,

we are in the same process here , porting an Ar1335 OnSemi on the I.mx8m Plus.

we have en NDA with nxp and are part of the beta program for the 8mp ,

could we get the same file ? And if any , some files and doc relative to this port ? 

my email is visible for you in my account i guess , if not , let me know. 

best regard,

Jeremie bours 

 

0 Kudos

1,179 Views
sachin_patel
Contributor III

Hi Jeremie, as NXP support is usually slow to respond, I thought I might as well at least help.

 

The table in the post I linked for the imx7 board has the same timing parameters, so if for example you want 1000 Mbps/lane, you choose HSSETTLE as 22.

1,182 Views
sachin_patel
Contributor III

Hi Jeremy, as NXP support is usually slow to respond, I thought I might as well at least help.

 

The table in the post I linked for the imx7 board has the same timing parameters, so if for example you want 1000 Mbps/lane, you choose HSSETTLE as 22.

1,160 Views
jeremie1
Contributor II

A great thank you Sachin ! 

We used the table accordingly, 

we are still stuck with uggly scrambled pixels, but that is the necessary pain when dealing with new camera  

 

400 x 480 RAW10 pixels , recorded in RGBP ( RGB565 ) by the I.MX8M plus :

image (24).png

The pixels seems not well aligned , if you had this kind of behaviour before, do not hesitate ! 
Best regard, and thank you again,

 

Jérémie

 

Tags (4)
0 Kudos

1,288 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sachin

 

file was sent via mail.

 

Best regards
igor

0 Kudos