i.MX 8M Nano: Linux Kernel: Operation points (CPUFreq)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX 8M Nano: Linux Kernel: Operation points (CPUFreq)

2,764 次查看
Svenifax
Contributor III

Hi NXP,

I found in the 5.4.24_2.1.0 Linux release for the i.MX 8M Nano that there are only three operation points supported: 1.2/1.4/1.5GHz.

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mn.dtsi?...

Device tree:

a53_opp_table: opp-table {
		compatible = "operating-points-v2";
		opp-shared;

		opp-1200000000 {
			opp-hz = /bits/ 64 <1200000000>;
			opp-microvolt = <850000>;
			opp-supported-hw = <0xb00>, <0x7>;
			clock-latency-ns = <150000>;
			opp-suspend;
		};

		opp-1400000000 {
			opp-hz = /bits/ 64 <1400000000>;
			opp-microvolt = <950000>;
			opp-supported-hw = <0x300>, <0x7>;
			clock-latency-ns = <150000>;
			opp-suspend;
		};

		opp-1500000000 {
			opp-hz = /bits/ 64 <1500000000>;
			opp-microvolt = <1000000>;
			opp-supported-hw = <0x100>, <0x3>;
			clock-latency-ns = <150000>;
			opp-suspend;
		};
	};

I want to have much lower frequencies, how can I archive that? Where can I found the regarding information in the data manuals? Like opp-microvolt and opp-supported-hw?

Best regards,
Sven

 

标签 (2)
0 项奖励
回复
4 回复数

2,761 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Svenifax,

 

These are the cpufreq that are available for the MX8MN and are part of kernel of the bsp, NXP don't have the opp/microvolt, however you can add more frequencies and add he opp-microvilt to it.

 

Regards

0 项奖励
回复

2,754 次查看
Svenifax
Contributor III

Hello NXP,

is there no information available about the missing infos?

To add an operating point, the relationship between frequency, voltage and register settings must be known.

This information should be part of the documentation. Where can I found this?

Best regards,
Sven

0 项奖励
回复

2,746 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hell, 

For all related to MX8MN in linux, You can view the Linux reference manual on your yocto documentation. otherwise you can view the reference manual of the chip.

 

Regards

0 项奖励
回复

2,742 次查看
Svenifax
Contributor III

Hello,

I checked the the following documents:

  • i.MX 8M Nano Applications Processor Datasheet for Industrial Products (IMX8MNIEC) - Rev. 1, 03/2021
  • i.MX 8M Nano Applications ProcessorReference Manual (IMX8MNRM) - Rev. 1, 11/2020
  • i.MX Linux Reference Manual (IMXLXR) - Rev. LF5.10.35_2.0.0, 30 June 2021

I could not found any information between the relationship of cpu frequency, voltage and register settings.

Where can I found such information?

Best regards,
Sven

 

0 项奖励
回复