i.MX 8M Nano LPDDR4 SOM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Nano LPDDR4 SOM

Jump to solution
852 Views
NATHANKLOGIC
Contributor III

I am wondering if there is a SOM available for purchase that uses the i.MX 8M Nano processor with LPDDR4.  There are reference schematics titled X-815LPD4-CPUCY on the Nano EVK webpage, but no mention of this SOM being available for purchase.  The EVK indicates it comes with a SOM that contains DDR4.

Thanks

Labels (1)
Tags (1)
0 Kudos
1 Solution
790 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nathan

for obtaining i.MX 8M Nano LPDDR4 SOM one can apply

to local sales office  Worldwide Locations | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
791 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nathan

for obtaining i.MX 8M Nano LPDDR4 SOM one can apply

to local sales office  Worldwide Locations | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------