I have a i.MX 8M Mini eva board and I downloaded the demo image from the website L4.14.98_2.0.0_MX8MM image from this link https://www.nxp.com/webapp/sps/download/preDownload.js
After I flash the image into the eMMc using UUU tool I realized that many packages on this image is missing such as apt-get, dpkg.
Anyone knows how to add those packages into this distribution or I have to recompile the kernel if so what document is the best to refer?
Hi Tang,
You could use the Linux dd command in the following way:
$ sudo dd if=<image name>.sdcard of=/dev/sd<partition> bs=1M && sync
For more information, you could refer to section 6.1 “Flashing an SD card image” of “Freescale Yocto Project User's Guide” document, from the L4.14.98_2.0.0_LINUX_DOCS package.
Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------
Hi Tang,
You could refer to the Release Notes of “L4.14.98_2.0.0_MX8MM” to ensure which features are included on the Yocto release.
In case of requiring custom or complementary features, like a package manager, you could take a look to the following Community thread:
Can we add Debian packages(Package_deb) in Yocto build?
Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------
Hi,
I finish the bitbake core-image-base process and then followed the steps to
flash the image to SD card
bunzip2 -dk -f bs=1M conv=fsync
Then my SD card says:
Unable to detect file system! Possible reasons are:
- The file system is damaged
- The file system is unknown to GParted
- There is no file system available (unformatted)
- The device entry /dev/mmcblk0p1 is missing
do you know why? I just format my SD card but I did not assign partitions
into it. I assume I can use the DD directly.
Just want to double check with a concept. Is that possible to add customized modules into the current running image on my device.Or I have to re compile a new image file.
Sent from my iPhone