i.MX 8M Mini Evaluation Kit SCH and PCB files for Altium Designer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 8M Mini Evaluation Kit SCH and PCB files for Altium Designer

ソリューションへジャンプ
1,169件の閲覧回数
Optergy-Pat
Contributor II

I've been trying to import the i.MX 8M Mini Evaluation Kit and SOM SCH and PCB files imported into Altium Designer. However, Altium keeps saying the files can't be imported. Do you have the SCH and PCB for the DDR4 and LPDDR4 versions that can be imported into Altium?

0 件の賞賛
返信
1 解決策
1,141件の閲覧回数
Yuri
NXP Employee
NXP Employee
0 件の賞賛
返信
5 返答(返信)
1,142件の閲覧回数
Yuri
NXP Employee
NXP Employee

Done!

0 件の賞賛
返信
1,148件の閲覧回数
Yuri
NXP Employee
NXP Employee

@Optergy-Pat 
Hello,

  I have sent You the design files directly.

Regards,
Yuri.

0 件の賞賛
返信
389件の閲覧回数
Stevef56
Contributor I

would it be possible to send those files to me as well? stevef56@hotmail.com

0 件の賞賛
返信
1,139件の閲覧回数
SJA
Contributor II

Can I get those files also.

Thanks

0 件の賞賛
返信
1,145件の閲覧回数
Optergy-Pat
Contributor II

Hi @Yuri ,

Thank you for sending the imx8m nano files and could you also please send me the files for the imx8m mini as well? Thank you.