i.MX 8M Mini Evaluation Kit SCH and PCB files for Altium Designer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Mini Evaluation Kit SCH and PCB files for Altium Designer

Jump to solution
1,417 Views
Optergy-Pat
Contributor II

I've been trying to import the i.MX 8M Mini Evaluation Kit and SOM SCH and PCB files imported into Altium Designer. However, Altium keeps saying the files can't be imported. Do you have the SCH and PCB for the DDR4 and LPDDR4 versions that can be imported into Altium?

0 Kudos
Reply
1 Solution
1,389 Views
Yuri
NXP Employee
NXP Employee
0 Kudos
Reply
5 Replies
1,390 Views
Yuri
NXP Employee
NXP Employee

Done!

0 Kudos
Reply
1,396 Views
Yuri
NXP Employee
NXP Employee

@Optergy-Pat 
Hello,

  I have sent You the design files directly.

Regards,
Yuri.

0 Kudos
Reply
637 Views
Stevef56
Contributor I

would it be possible to send those files to me as well? stevef56@hotmail.com

0 Kudos
Reply
1,387 Views
SJA
Contributor II

Can I get those files also.

Thanks

0 Kudos
Reply
1,393 Views
Optergy-Pat
Contributor II

Hi @Yuri ,

Thank you for sending the imx8m nano files and could you also please send me the files for the imx8m mini as well? Thank you.