i.MX 8M Mini 1440*1440 Display Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Mini 1440*1440 Display Support

Jump to solution
639 Views
balogul
Contributor I

Hi,

We are designing a device that will run on Android 13 OS with the i.MX 8M Mini. According to the datasheet it supports up to 1080p (1080*1920) 60fps display through MIPI DSI.

I assume that it could support 1440*1440 display with 60 fps as well since total number of pixels are the same for both but I wanted to be sure before we move forward.

Thanks.

0 Kudos
Reply
1 Solution
603 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @balogul,

I hope you are doing well.

Yes, you are right, Your logic makes sense in terms of total pixel count.
In general, resolution support is determined by the display controller and the associated drivers.

->While the total pixel count might be the same for both 1080p (1080x1920) and 1440x1440 displays, there are other factors to consider, such as aspect ratio, pixel clock frequency, and the ability of the MIPI DSI interface to handle the desired resolution.

It is not supported, only supported pixel formats are mentioned in the above thread.

I hope this answers your query.

Thanks & Regards,
Sanket Parekh

View solution in original post

0 Kudos
Reply
6 Replies
618 Views
balogul
Contributor I

Hi @Sanket_Parekh,

Thank you for your response. I hope you are doing well too.

So, it also supports 1440*1440 pixel display as well, correct?

Thanks.

0 Kudos
Reply
612 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @balogul,

I hope you are doing well.

So, it also supports 1440*1440 pixel display as well, correct?
->No, It will only support as mentioned in the above thread.

I hope this answers your query.

Thanks & Regards,
Sanket Parekh

0 Kudos
Reply
607 Views
balogul
Contributor I
Hi,

I appreciate the help.

1080p means 1080*1920 pixels which is equal to the number of pixels for 1440*1440 display. Technically, if it supports one it should support the other as well.
So I would appreciate if you can double check this information.

Thanks.
0 Kudos
Reply
604 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @balogul,

I hope you are doing well.

Yes, you are right, Your logic makes sense in terms of total pixel count.
In general, resolution support is determined by the display controller and the associated drivers.

->While the total pixel count might be the same for both 1080p (1080x1920) and 1440x1440 displays, there are other factors to consider, such as aspect ratio, pixel clock frequency, and the ability of the MIPI DSI interface to handle the desired resolution.

It is not supported, only supported pixel formats are mentioned in the above thread.

I hope this answers your query.

Thanks & Regards,
Sanket Parekh

0 Kudos
Reply
597 Views
balogul
Contributor I
Hi, thank you for the help.
Best,
0 Kudos
Reply
627 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @balogul,

I hope you are doing well.

"According to the datasheet it supports up to 1080p (1080*1920) 60fps display through MIPI DSI."
->Yes, you are right it has the "Multimedia" subsystem that includes below features.

Video Processing Unit:
• 1080p60 VP9 Profile 0, 2 (10-bit)
• 1080p60 HEVC/H.265 Decoder
• 1080p60 AVC/H.264 Baseline, Main, High decoder
• 1080p60 VP8
• 1080p60 AVC/H.264 Encoder
• 1080p60 VP8
• TrustZone support

Graphic Processing Unit:
• GCNanoUltra for 3D acceleration
• GC320 for 2D acceleration

LCDIF Display Controller:
• Support up to 2 layers of overlay
• Support up to 1080p60 display through MIPI DSI

MIPI Interface:
• 4-lane MIPI CSI interface
• 4-lane MIPI DSI interface

Audio:
• S/PDIF input and output, including a new Raw Capture input mode
• Five synchronous audio interface (SAI) modules supporting I2S, AC97, TDM, codec/DSP, and DSD interfaces, including one SAI with 8 Tx and 8 Rx lanes, one SAI with 4 Tx and 4 Rx lanes, two SAI with 2 Tx and 2 Rx lanes, and one SAI with 1 Tx and 1Rx lane. Support over 20 channels of audio subject to I/O limitations.
• 8-Channel Pulse Density Modulation (PDM) input

Thanks & Regards,
Sanket Parekh

0 Kudos
Reply