We got some "panel PC" from China what has NXP i.MX 8M Mini, with system image running:
"Linux imx8mmevk 5.10.72-lts-5.10.y+g2a23c0cdbb9b #1 SMP PREEMPT Tue Oct 25 12:05:04 UTC 2022 aarch64 aarch64 aarch64 GNU/Linux"
with toolchain named:
"fsl-imx-wayland-glibc-x86_64-core-image-base-cortexa53-crypto-imx8mmevk-toolchain-5.10-hardknott"
GPIO is accessed via sysfs, but if I run this test script:
while true;
do
for I in {04..11};
do
cat "/sys/class/gpio/gpio5${I}/value";
done;
done
After some (random) time I am starting to get errors, losing ability to read GPIO values:
cat: /sys/class/gpio/gpio504/value: Resource temporarily unavailable
cat: /sys/class/gpio/gpio505/value: Resource temporarily unavailable
cat: /sys/class/gpio/gpio506/value: Resource temporarily unavailable
cat: /sys/class/gpio/gpio507/value: Resource temporarily unavailable
cat: /sys/class/gpio/gpio508/value: Resource temporarily unavailable
cat: /sys/class/gpio/gpio509/value: Resource temporarily unavailable
cat: /sys/class/gpio/gpio510/value: Resource temporarily unavailable
cat: /sys/class/gpio/gpio511/value: Resource temporarily unavailable
It seems that to fix this issue I have to turn off device completely, hot system reboot does not help.
Not sure what to thing about it, could it be some buggy custom Chinese kernel code, bug in NXP kernel, or just bad board (electronics) design so that GPIO goes haywire after some random glitch?
Thanks!
# ulimit -a
real-time non-blocking time (microseconds, -R) unlimited
core file size (blocks, -c) 0
data seg size (kbytes, -d) unlimited
scheduling priority (-e) 0
file size (blocks, -f) unlimited
pending signals (-i) 5218
max locked memory (kbytes, -l) 64
max memory size (kbytes, -m) unlimited
open files (-n) 1024
pipe size (512 bytes, -p) 8
POSIX message queues (bytes, -q) 819200
real-time priority (-r) 0
stack size (kbytes, -s) 8192
cpu time (seconds, -t) unlimited
max user processes (-u) 5218
virtual memory (kbytes, -v) unlimited
file locks (-x) unlimited
Hi @VincasD
Hi @VincasD,
Hi @VincasD,
I hope you are doing well
To read/write the gpio using this sysfs interface is being deprecated. We recommend you use the 'gpiod' method. One can read the value of gpio using the command gpioget.
I have tested the reading and writing the gpio in the loop for a long time using the script you are implementing by using the above command. Here we were unable to reproduce the error. It worked fine for us.
In our case, we used board IMX8M mini, BSP version - 6.1.1.
Thanks & Regards,
Sanket Parekh
I've found code that enables sysfs - removed id, and now we are using gpiod (VTGLinuxIO is our daemon):
# ./gpioinfo gpiochip5
gpiochip5 - 16 lines:
line 0: unnamed unused input active-high
line 1: unnamed unused input active-high
line 2: unnamed unused input active-high
line 3: unnamed unused input active-high
line 4: unnamed unused input active-high
line 5: unnamed unused input active-high
line 6: unnamed unused input active-high
line 7: unnamed unused input active-high
line 8: unnamed "VTGLinuxIO" input active-high [used]
line 9: unnamed "VTGLinuxIO" input active-high [used]
line 10: unnamed "VTGLinuxIO" input active-high [used]
line 11: unnamed "VTGLinuxIO" input active-high [used]
line 12: unnamed "VTGLinuxIO" input active-high [used]
line 13: unnamed "VTGLinuxIO" input active-high [used]
line 14: unnamed "VTGLinuxIO" input active-high [used]
line 15: unnamed "VTGLinuxIO" input active-high [used]
But even with gpiod we have issues: time to time line gets unreadable (and we assert and intentionaly abort), and we see "kernel: pca953x 2-0020: failed reading register" error printed in journal:
Sep 05 13:40:40 imx8mmevk VTGGPIOService[6007]: Failed to open LinuxIO device: "Resource temporarily unavailable (system:11)"
Sep 05 13:40:40 imx8mmevk kernel: pca953x 2-0020: failed reading register
Sep 05 13:40:40 imx8mmevk kernel[276]: [ 8292.357291] pca953x 2-0020: failed reading register
Sep 05 13:40:40 imx8mmevk systemd[1]: VTGGPIOService.service: Main process exited, code=exited, status=1/FAILURE
Maybe it's wrong driver, or too old driver, etc? Any ideas?
No it's really not the processes issue, same POSIX error code might be use AND for process limits, yes, but I get these errors randomy before GPIO fully hangs. There's less than 200 threads on the system, while:
max user processes (-u) 1312
After night I can run new processes, etc, all works, bug GPIO is completely stuck until cold restart:
# for PIN in {8..15}; do echo "Reading gpiochip5 pin $PIN"; ./gpioget gpiochip5 $PIN; done
Reading gpiochip5 pin 8
./gpioget: error reading GPIO values: Resource temporarily unavailable
Reading gpiochip5 pin 9
./gpioget: error reading GPIO values: Resource temporarily unavailable
Reading gpiochip5 pin 10
./gpioget: error reading GPIO values: Resource temporarily unavailable
Reading gpiochip5 pin 11
./gpioget: error reading GPIO values: Resource temporarily unavailable
Reading gpiochip5 pin 12
./gpioget: error reading GPIO values: Resource temporarily unavailable
Reading gpiochip5 pin 13
./gpioget: error reading GPIO values: Resource temporarily unavailable
Reading gpiochip5 pin 14
./gpioget: error reading GPIO values: Resource temporarily unavailable
Reading gpiochip5 pin 15
./gpioget: error reading GPIO values: Resource temporarily unavailable
Could you please share the device tree file you are using for further debugging the issue?
Where do I find it?
Also please confirm that if you were able to read these gpio values from the terminal without using the for loop in the script or not.
We do read values successfully in our "gpio service" application (using QFile), and I do see values changing in /sys/kernel/debug/gpio. Simply after some time of running I can no longer read values - does not matter is it our Qt application or `cat` in terminal.
I've built gpiod utilities and I see this:
# ./gpioinfo gpiochip5
gpiochip5 - 16 lines:
line 0: unnamed unused input active-high
line 1: unnamed unused input active-high
line 2: unnamed unused input active-high
line 3: unnamed unused input active-high
line 4: unnamed unused input active-high
line 5: unnamed unused input active-high
line 6: unnamed unused input active-high
line 7: unnamed unused input active-high
line 8: unnamed "sysfs" input active-high [used]
line 9: unnamed "sysfs" input active-high [used]
line 10: unnamed "sysfs" input active-high [used]
line 11: unnamed "sysfs" input active-high [used]
line 12: unnamed "sysfs" input active-high [used]
line 13: unnamed "sysfs" input active-high [used]
line 14: unnamed "sysfs" input active-high [used]
line 15: unnamed "sysfs" input active-high [used]
I see [used] inputs market as sysfs, maybe that's the ones I am using. But it's [used] even while there is no my script, nor my application running that would access GPIO, so could this mean as you said - that something else are using them?
Not sure about "checking device tree" though..?