i.MX 8 opencv videocapture very slow (video file)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8 opencv videocapture very slow (video file)

8,029 Views
alan13341313
Contributor I

alan13341313_0-1617868686876.png

For videocaptrue.read takes about 190ms per frame

Can someone tells me which part have I missed?

 

0 Kudos
Reply
10 Replies

6,903 Views
aekam_parmar
Contributor II

Hey,

This is similar to the problem I am facing right now, and it is reported HERE.

@gnar_fang I created an OpenCV application that uses the GStreamer pipeline to play an MP4 file, but the CPU consumption is high.

@Zhiming_Liu as you mentioned that hardware acceleration is not imported in OpenCV. Based on similar performance issues, I assume it is not imported into the Qt framework either. Please share steps to import/enable hardware acceleration for OpenCV and Qt.

 

I am planning to create an application using the Qt framework on i.MX8M Plus EVK.

As per the Yocto document, Qt6 is built/provided with the full image, but Qt6 does not support providing gstreamer pipeline (explicitly) to QMediaPlayer class.

So all I can do is rely on the internal pre-defined pipeline it has or constructs at run-time. Not sure if it uses hardware components.

 

Looking forward to your response.

0 Kudos
Reply

6,892 Views
gnar_fang
NXP Employee
NXP Employee

Currently, G2D doesn't integrate into OpenCV.

If you use IMX8MP, you can try G2D and OpenCL with GStreamer pipeline to 

get video frames. In my demo, the CPU loading can reduce to less than 10%.

https://github.com/fangxiaoying/opencl_study/blob/main/gst_case/open_camera_v3.cc

This is research from a long time ago, and threre questions that can be discussed.

0 Kudos
Reply

7,986 Views
alan13341313
Contributor I

1. Build yocto and use.wic file inside yocto for SD card here's the steps

sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib build-essential chrpath socat cpio python python3 python3-pip python3-pexpect xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev pylint3 xterm
mkdir ~/bin
curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
chmod a+x ~/bin/repo
export PATH=~/bin:$PATH
sudo apt-get install repo
git config --global user.name xxx
git config --global user.email xxx@gmail.com
git config --list
mkdir imx-yocto-bsp
cd imx-yocto-bsp
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.70-2.3.0.xml
repo sync
DISTRO=fsl-imx-xwayland MACHINE=imx8mpevk source imx-setup-release.sh -b build-yocto
bitbake imx-image-full

run this inside iMX8  (weston --tty=1 --device=/dev/fb0,/dev/fb2 --use-g2d=1 &)

2. Use aarch64-poky to build a simple opencv videoCapture read a frame a imshow for output

and scp into iMX then  ./test test.mp4

0 Kudos
Reply

8,026 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Can you share your steps?

0 Kudos
Reply

8,010 Views
alan13341313
Contributor I

1. Build yocto

sudo apt-get install gawk wget git-core diffstat unzip texinfo gcc-multilib build-essential chrpath socat cpio python python3 python3-pip python3-pexpect xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev pylint3 xterm
mkdir ~/bin
curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
chmod a+x ~/bin/repo
export PATH=~/bin:$PATH
sudo apt-get install repo
git config --global user.name davison
git config --global user.email davison12071994@gmail.com
git config --list
mkdir imx-yocto-bsp
cd imx-yocto-bsp
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.70-2.3.0.xml
repo sync
DISTRO=fsl-imx-xwayland MACHINE=imx8mpevk source imx-setup-release.sh -b build-yocto
bitbake imx-image-full

2. SD card

use .wic file in yocto for sd card

3. Run on iMX 8

run this in iMX8 (weston --tty=1 --device=/dev/fb0,/dev/fb2 --use-g2d=1 &)

Build a simple program by aarch64-poky and scp into iMX8 then ./test

 

 

Here's the code

#include "opencv2/opencv.hpp"
#include <iostream>

using namespace std;
using namespace cv;

int main(){

// Create a VideoCapture object
VideoCapture cap("test.mp4");

// Check if camera opened successfully
if(!cap.isOpened()){
cout << "Error opening video stream" << endl;
return -1;
}

while(1){

Mat frame;

// Capture frame-by-frame
cap >> frame;

// If the frame is empty, break immediately
if (frame.empty())
break;

// Display the resulting frame
imshow( "Frame", frame );

// Press ESC on keyboard to exit
char c = (char)waitKey(1);
if( c == 27 )
break;
}

// When everything done, release the video capture
cap.release();

// Closes all the frames
destroyAllWindows();
return 0;
}

0 Kudos
Reply

8,017 Views
alan13341313
Contributor I

Code looks like 95% like this

 

#include "opencv2/opencv.hpp"
#include <iostream>

using namespace std;
using namespace cv;

int main(){

  // Create a VideoCapture object
  VideoCapture cap("test.mp4"); 

  // Check if camera opened successfully
  if(!cap.isOpened()){
   	cout << "Error opening video stream" << endl;
        return -1;
  }
while(1){ Mat frame; // Capture frame-by-frame cap >> frame; // If the frame is empty, break immediately if (frame.empty()) break; // Display the resulting frame imshow( "Frame", frame ); // Press ESC on keyboard to exit char c = (char)waitKey(1); if( c == 27 ) break; } // When everything done, release the video capture cap.release(); // Closes all the frames destroyAllWindows(); return 0; }

 

0 Kudos
Reply

7,885 Views
gnar_fang
NXP Employee
NXP Employee

I am not sure which camera are you used.  it may need GStreamer plugin to accelerate image decode.

For example. open ov5640

if you can open camera with the command.

$ gst-launch-1.0 v4l2src device=/dev/video1 ! video/x-raw,framerate=30/1 width=1920,height=1080! waylandsink

for OpenCV, you can use the code to open camera.

const std::string pipeline = "v4l2src device=/dev/video3 ! video/x-raw,framerate=30/1, width=1920,height=1080 ! appsink";

cam = cv::VideoCapture(pipeline,cv::CAP_GSTREAMER);

 

for MJPG or other encoded formats need to add VPU / G2D plugin in the pipeline.

0 Kudos
Reply

8,003 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

OK,i will test it and give you feeback

0 Kudos
Reply

7,974 Views
alan13341313
Contributor I

Hi there, any solution? Or is there a way to use gstreamer in code to replace videocapture

0 Kudos
Reply

7,963 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You can try to use gstreamer, we don't import hardware acceleration in opencv 

0 Kudos
Reply