i.MX 7ULP industrial variant vs. EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 7ULP industrial variant vs. EVK

381 Views
Nico_H
Contributor II

Hello,

we have evaluated the i.MX 7ULP EVK and developed a new board with the industrial variant MCIMX7U5CVP06SD.

Now we are running almost the same BSP on the new board with a frequency of 720 MHz for A7 processor and 352,8 MHz for LPDDR3.

The datasheet of the industrial version noticed a maximum of 650 MHz for A7 and 271,5 MHz for LPDDR3. It seems to run stable (for now), but are there conditions where it could get into an unstable state? Maybe at lower temperatures?

Why is the maximum frequency of the industrial version lower than the consumer variant?

 

Kind regards,

Nico H.

Labels (1)
0 Kudos
Reply
1 Reply

365 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, for the maximum frequency of the industrial version lower than the consumer variant. But for the Junction Temperature Range is higher than the consumer. Details please refer to our datasheet.

0 Kudos
Reply