i.MX 7Dual SABRE Board demo image epdc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 7Dual SABRE Board demo image epdc

1,244 Views
hiroyukihara
Contributor III

"Demo Images - SABRE Board based on i.MX 7 Dual" has u-boot / boot / recovery epdc version, but what is different?
How can I build the epdc version?

I will transfer it to a different EPD for IMXEBOOKDC4.
And fix mxc_epdc_fb.c.
How do you build an epd version?

0 Kudos
2 Replies

922 Views
igorpadykov
NXP Employee
NXP Employee

Hi hiroyuki

please include epdc driver as described in Chapter 10 Electrophoretic Display Controller

(EPDC) Frame Buffer Driver attached Linux Manual and use

Table 10. Common kernel boot parameters attached Release Notes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

922 Views
hiroyukihara
Contributor III

I saw Chapter 10 of the i.MX Linux® Reference Manual.

However, we did not need to change anything except support for splash screen.
Enable below
#define CONFIG_SPLASH_SCREEN
#define CONFIG_MXC_EPDC

Is the epdc version of "Demo Images - SABRE Board based on i.MX 7 Dual" supporting splash screen support?

Moreover, I do not understand the following method.

10.3.7 Enabling an EPDC Splash Screen
 3. Write the firmware file to the SD card at the FAT partition.
     cp epdc_E060SCM.bin [FAT partition on SD card]

The following is the partition of the SD card.
Where can I make a FAT partition and copy it?

Create a new partition with sdb13 with FAT,
Is it OK with the operation below?
> sudo mount/dev/sdb13/mnt
> sudo cp epdc_E060SCM_splash.bin /mnt/epdc_E060SCM.bin
> sudo umount /mnt

pastedImage_1.png

0 Kudos