i.MX 6UltraLite power consumption issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6UltraLite power consumption issue

597 Views
liyingchun
Contributor I

Hi expert

I have a i.MX 6UltraLite question:I want to design a low power consumption production using i.MX 6UltraLite processor and need the deep sleep funtion for this processor. When entering deep sleep funtion the current should be less than 4mA. Does this processer meets this requirement? Is there any document about the power management of this chip?

Thanks very much!

Tags (1)
0 Kudos
1 Reply

349 Views
igorpadykov
NXP Employee
NXP Employee

HI li

yes processor itself meets this requirement,

for deep sleep mode current one can look at AN5170

i.MX 6UltraLite Power Consumption Measurement

i.MX 6UltraLite Applications Processor|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos