i.MX 6UltraLite EVK Board SDR104

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6UltraLite EVK Board SDR104

2,630 Views
peterscharpf
Contributor I

Is  the i.MX 6UltraLite EVK Board capable of running at SDR104 speeds from SD1?

I realize the iMX6 UL is capable of SDR104 speeds but has the i.MX 6UltraLite EVK Board been tested at or has anyone had success running the board at SDR104 speeds?

Tags (1)
0 Kudos
Reply
2 Replies

1,206 Views
marcowang
Contributor II

Hi Igor,

Could you please share me test procedure and result ? Tks 

0 Kudos
Reply

1,206 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

yes it was tested and I can share results.

Please create service request.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply