i.MX 6ULL voltage supplies

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6ULL voltage supplies

453 Views
rprronad
Contributor IV

Dear Experts,

The i.MX 6ULL processors have several power supply domains (voltage supply rails) and multiple internal power domains. Is there any way to check the voltage supply rails through a Linux command if these values are stored in registers or elsewhere?

Please provide me with information on whether it is possible to see the voltage rails via a Linux command.

 

Thanks & Regards

Ravikumar 

0 Kudos
Reply
4 Replies

416 Views
rprronad
Contributor IV

Thank you for your response and inputs.

Is there a method to capture the power monitoring for the i.MX6ULL?

Or, how can I implement a method to monitor the power rails? Any guidance on this would be greatly appreciated.


Thanks & Regards, 

Ravikumar

0 Kudos
Reply

325 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

As is mentioned by roke, you can check the configured value in:

/sys/class/regulator/* ; do cat $i/name; cat $i/microvolts; echo; done

This is how is done in hardware on i.MX93EVK board.

Best regards.

380 Views
roke
Contributor III

linux-imx/Documentation/ABI/testing/sysfs-class-regulator at lf-5.15.71-2.2.0 · nxp-imx/linux-imx · ...

kernel.org/doc/Documentation/ABI/testing/sysfs-class-regulator

 

If you add the regulators correctly, you will find in /sys/class/regulator. 

Again. the premise is to add the regulator correctly.

 

426 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

This should be done by hardware, adding power monitors for each power rail in the processor. We have similar solutions in other boards such as i.MX8MPEVK, i.MX8ULP, i.MX93EVK, etc. And the monitoring is done through our BCU tool.

Unfortunately, i.MX6ULL is not supported on this tool and the data sent from power monitor should be captured an interpreted in your side.

Best regards.

0 Kudos
Reply