i.MX 6ULL Y1 and Y7 variants - Ethernet interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6ULL Y1 and Y7 variants - Ethernet interface

Jump to solution
1,043 Views
manuel_soledge
Contributor II

Hi NXP Community,

looking at the i.MX 6ULL Applications Processors for Consumer Products (IMX6ULLCEC.pdf) datasheet it shows that the Y1 and Y7 parts only have one Ethernet interface (Table 1, page 3-5).

However I can't find details on the pins that can be used by this interface. Does it correspond to the first or second interface of the full-feature Y2 variant?

Best,

Manuel

Labels (2)
0 Kudos
Reply
1 Solution
1,029 Views
igorpadykov
NXP Employee
NXP Employee

Hi Manuel

 

it is first interface.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
2 Replies
1,030 Views
igorpadykov
NXP Employee
NXP Employee

Hi Manuel

 

it is first interface.

 

Best regards
igor

0 Kudos
Reply
1,019 Views
manuel_soledge
Contributor II

Thank you very much !

Best regards,
Manuel

0 Kudos
Reply