Hi All,
I am following the document "i.MX Yocto Project User's Guide.pdf".
I have set up the development environment, e.g.
$ mkdir imx-yocto-bsp$ cd imx-yocto-bspm imx-4.9.88-2.0.0_ga.xml$ repo sync
etc..
Once I have done this, I see a note in the document ~/imx-yocto-bsp/README-IMXBSP
Note Qt is not supported on i.MX 6UltraLite and i.MX 7Dual. It works on X11 backend only but is not a supported feature.
My questions are:
Thanks,
Brian.
Hi Brian,
We have ported QT5.6.2 on our MYD-Y6ULX board, but imx6UL can not support GPU and hardware graphics.
It can only display from software but video effects might not too strong.
MEasy HMI QT Demo on i.MX6UL/6ULL MYD-Y6ULX Development Board - YouTube
Best regards,
Linda
And how to build yocto for imx6ull with qt5 and cross-compile qt application for it(or maybe better to compile it on the board)?
Hi Brian
i.MX6ULL is reduced version of i.MX6UL and it is also not supported,
as described in sect.2.1 New features attached Release Notes:
Qt 5 is not supported for SoCs without hardware graphics. Qt 5 video is not supported on SoCs without a VPU.
i.MX Family Matrix
https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------