i.MX 6ULL ADC usage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6ULL ADC usage

Jump to solution
1,433 Views
sugiyamatoshihi
Contributor V

Hi, 

I have a question about how to use ADC of i.MX 6ULL.

When I checked IOMUXC_SW_MUX_CTL_PAD_GPIO1_IO01 register in Reference manual. There is no ADC selection in MUX_MODE.

Should it select GPIO1_IO01 ALT5 in MUX_MODE for ADC input?

Best Regards,

Sugiyama

Labels (1)
0 Kudos
Reply
1 Solution
1,287 Views
art
NXP Employee
NXP Employee

There is no special IOMUX mode for the ADC input in the IOMUX Pad Configuration register since the ADC inputs are always connected to the corresponding pads. To minimize the possible signal contention and measurement error, the ADC input pad should be configured as GPIO (ALT5) input with no pull-up/pull-down/keeper circuit enabled.

Best Regards,

Artur

View solution in original post

0 Kudos
Reply
1 Reply
1,288 Views
art
NXP Employee
NXP Employee

There is no special IOMUX mode for the ADC input in the IOMUX Pad Configuration register since the ADC inputs are always connected to the corresponding pads. To minimize the possible signal contention and measurement error, the ADC input pad should be configured as GPIO (ALT5) input with no pull-up/pull-down/keeper circuit enabled.

Best Regards,

Artur

0 Kudos
Reply