i.MX 6SoloX SABRE Board's ping is slow.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6SoloX SABRE Board's ping is slow.

425 Views
toshinariagata
Contributor III

Hi,

I am using i.MX 6SoloX SABRE Board and i.MX 6Quad SABRE Board.
i.MX 6Quad SABRE Board's ping time is about 0.5 ms.
However, i.MX 6SoloX SABRE Board's ping time is about 1.7 ms.

Why is i.MX 6SoloX SABRE Board's ping slow?

0 Kudos
1 Reply

373 Views
art
NXP Employee
NXP Employee

The ping is slower on the i.MX6SoloX processor than on the i.MX6Quad processor just because the OS operates slower on i.MX6SoloX than on i.MX6Quad since i.MX6SoloX has only one CPU core whereas i.MX6Quad has 4 CPU cores.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos