i.MX 6SoloX M4 Ethernet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6SoloX M4 Ethernet

Jump to solution
815 Views
mirkoardinghi1
Contributor IV

I have an i.MX 6SoloX and I want to use the ethernet device with the M4 core, but in the MQX and in FreeRTOS too I cannot find any ethernet driver in these SO.

Is possible to manage the ethernet device with M4?

Labels (2)
0 Kudos
1 Solution
544 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Basically the ENET can be used with the CM4 core, please look at sections
“CM4 memory map” and “RDC Peripheral Mapping” of the i.MX6 SX RM.
But the RTOS does not support ENET.

 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
545 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Basically the ENET can be used with the CM4 core, please look at sections
“CM4 memory map” and “RDC Peripheral Mapping” of the i.MX6 SX RM.
But the RTOS does not support ENET.

 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------