i.MX 6Solo timing between DQS and DQ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6Solo timing between DQS and DQ

Jump to solution
934 Views
sesmor
Contributor II

Hello NXP!

I need to know t1 and t2 timings, I was trying to find this information in JESD79-3D standart and I couldn't do it. I need DQS out to earliest valid DQ/DM time in writing cycle and DQS out to latest valid DQ/DM time in writing cycle. Can you give me this timings? I have i.MX 6Solo controller (partnumber: MCIMX6S7CVM08AC). DDR3l-800 (AC160/DC90).
IMG_20170816_130514.jpg

0 Kudos
1 Solution
700 Views
igorpadykov
NXP Employee
NXP Employee

yes MMDC module is same for both processors.

~igor

View solution in original post

5 Replies
700 Views
igorpadykov
NXP Employee
NXP Employee

Hi Roman

one can check Table 43. DDR3/DDR3L Write Cycle i.MX6DQ Datasheet

http://www.nxp.com/docs/en/data-sheet/IMX6DQCEC.pdf 

and tDQSS, tDSS parameters in Figure 44 — Write

Timing Definition and Parameters in JESD79  DDR3 specification

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
700 Views
sesmor
Contributor II

No, Table 43 from datasheet showing timings for flash memory, that is not what i needed. tDQSS and tDSS are not the timings I need, because that timings showing how DQS is refering to CK, I need timings showing how DQS is refering to DQ (I showed needed timings in the picture in the first massage). Снимок.PNG

0 Kudos
700 Views
igorpadykov
NXP Employee
NXP Employee

pastedImage_1.jpg

700 Views
sesmor
Contributor II

This datasheet (IMX6DQCEC) is for I.MX 6Dual/6Quad, I have i.MX 6Solo (IMX6SDLIEC). Do they have the same timings?

0 Kudos
701 Views
igorpadykov
NXP Employee
NXP Employee

yes MMDC module is same for both processors.

~igor