i.MX 6DualLite: is it capable of using a 1920x1200 LCD display?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6DualLite: is it capable of using a 1920x1200 LCD display?

Jump to solution
823 Views
gabrielvalcazar
Contributor IV

Good afternoon,

We have a client that has implemented our i.MX 6DualPlus-based SOM on their product. Their user interface requires the use of an 1920x1200 LCD display connected to the SOM via a parallel 24-bit display port. So far this implementation is working correctly, but now they are looking to create an alternative version of this product using our i.MX 6DualLite-based SOM instead of the 6DualPlus, but they're not sure if that SOC supports the resolution of their LCD display. We currently don't have the hardware necessary to test this for ourselves, so it would be great to get an official statement on this.

According to the i.MX6/i.MX7 family comparison table, the maximum LCD display resolution supported by the 6DualLite is 1280x720: https://www.nxp.com/docs/en/brochure/FLYRIMXPRDCMPR.pdf

However, a colleague of mine found the following text in the i.MX 6Solo/6/DualLite Applications Processor Reference Manual (page 203):

Each i.MX 6Solo/6DualLite processor enables the following interfaces to external
devices (some of them are muxed and not available simultaneously):
• Displays—Total four interfaces available. Total raw pixel rate of all interfaces is up
to 266 Mpixels/sec, 24 bpp. Up to three interfaces may be active in parallel
(excluding EPDC).
• One Parallel 24-bit display port, up to 225 Mpixels/sec (for example, WUXGA at 60
Hz or dual HD1080 and WXGA at 60 Hz)
• LVDS serial ports—One port up to 170 Mpixels/sec or two ports up to 85 MP/sec
(for example, WUXGA at 60 Hz) each
• HDMI 1.4 port
• MIPI/DSI, two lanes at 1 Gbps
• EPDC, Color, and monochrome E-INK, up to 1650x2332 resolution and 5-bit
grayscale

It mentions that the 24-bit parallel display port could support WUXGA, but I assume this is just an example of a mode that can be achieved with the interface's bitrate, rather than an actual mode that is supported by the SOC.

In short: is the i.MX 6DualLite capable of using a resolution of 1920x1200 for an LCD display via a 24-bit parallel port?

Many thanks in advance and best regards,

Gabriel

Labels (1)
0 Kudos
Reply
1 Solution
815 Views
jamesbone
NXP TechSupport
NXP TechSupport

Yes, you are correct, this is just an example of the maximum resolution that can be handle based on the BitRate of the interface. This means that can be supported this resolution if only one LCD interface it is handle and it is the only media no other camera, or device over the IPU that rest the BitRate of the interface.

But I need to said that can be accomplished, but I suggest if this resolution need to be handle then migrate to the i.MX8M or the i.MX8M Mini. Which handle this resolution as base.

 

 

View solution in original post

0 Kudos
Reply
1 Reply
816 Views
jamesbone
NXP TechSupport
NXP TechSupport

Yes, you are correct, this is just an example of the maximum resolution that can be handle based on the BitRate of the interface. This means that can be supported this resolution if only one LCD interface it is handle and it is the only media no other camera, or device over the IPU that rest the BitRate of the interface.

But I need to said that can be accomplished, but I suggest if this resolution need to be handle then migrate to the i.MX8M or the i.MX8M Mini. Which handle this resolution as base.

 

 

0 Kudos
Reply