Hello,Team:
I'm using fsl-imx6 board with i.MX 6Dual Processor,and i download the demo binary form L4.14.78_1.0.0_MX6QDLSOLOX .I try to burn with the downloaded binary(fsl-image-validation-imx-imx6qpdlsolox.sdcard and u-boot-imx6dlsabresd_sd.imx),but the process abort after a while.
In addition,I've not found out imx6dsabresd.conf but imx6dlsabresd.conf in machine directory.what's difference between imx6dsabresd and imx6dlsabresd.
Thank you.
Hello,
I see by the image you share that you are using UUU to flash your board,
Could you share the script that you're using (UUU.auto)?
In your case you'll need to rename the uuu.auto-imx6dlsabresd to uuu.auto, place it inside the zip file and run the command:
.\uuu.exe L4.14.78_1.0.0_ga_images_MX6QPDLSOLOX.zip
This will burn the yocto image to the eMMC
Hope this helps,
Best regards,
Aldo.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello,
I try to change the u-boot image (from u-boot-imx6dlsabresd_sd.imx to u-boot-imx6qsabresd_sd.imx) ,and sloven this problem.
Thank you.
Hello,
Thank you for sharing how you solved this with everyone,
Best regards,
Aldo.