i.MX 6Dual/6Quad HDMI and VGA can not read edid data with i2c.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 6Dual/6Quad HDMI and VGA can not read edid data with i2c.

530件の閲覧回数
zhengguang_yang
Contributor II

Linux:3.14.28

The default EDID is from the device tree.Whether 3.14.28 linux does not support the acquisition of EDID from I2C

0 件の賞賛
1 返信

418件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

it is working fine with nxp official linux releases

i.MX 6 Series Software and Development Tool|NXP 

please check if proper HDMI cable used, check that you use "true"

HDMI or just a HDMI - DVI adapter.
"True" HDMI display with special HDMI cable should be used.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛