i.MX 6D 16bit single DDR3 chip support?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6D 16bit single DDR3 chip support?

670 Views
zrshnsh
Contributor I

Hi, we are using i.MX 6d processor with two DDR3 chips to make a 32bit RAM access.

Now we want to save the cost of our BOM, so we tried to using single chip of DDR3 chip, that is 16bit RAM access.

We removed one DDR3 chip from our board, used I.MX6DQSDL DDR3 Script Aid to generate script for ddr stress tester.

Catch0B4F(12-12-10-48-08).jpg

Catch(12-12-10-48-08).jpg

But this does not work at all, We got error "DCD addr is out of valid range" if we check the "Verify DCD Address" box option in the DDR Test Tool. If it is not checked we got a "Write dcd failed" error.

So, we want to ask if anyone knows does i.MX 6d support 16bit single DDR3 chip to work with? Thanks a lot!

Labels (1)
Tags (1)
0 Kudos
1 Reply

453 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ran

error "DCD addr is out of valid range." is described in faq section on:

i.MX6/7 DDR Stress Test Tool V2.92 

16 bit configuration is supported according to sect.44.12.1 MMDC Core Control

Register (MMDCx_MDCTL) i.MX6DQ Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos