i.MX 6 SL L3.0.35_2.1.0 Release

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 6 SL L3.0.35_2.1.0 Release

2,122件の閲覧回数
EnriqueOchoaVaz
Contributor V

Hi All,

The new i.MX 6 SL L3.0.35_2.1.0 release is now available on the http://www.freescale.com/site.

·         Files available

#

Name

Description

1

L3.0.35_2.1.0_LINUX_DOCS

i.MX   6SoloLite Linux BSP Documentation. Includes Release Notes, Reference Manual,   User guide. API Documentation

2

L3.0.35_2.1.0_LINUX_MMDOCS

i.MX 6SoloLite Linux Multimedia Codecs   Documentation. Includes   CODECs Release Notes and User's Guide

3

L3.0.35_2.1.0_ER_SOURCE

i.MX   6SoloLite Linux BSP Source Code Files

4

L3.0.35_2.1.0_MM_CODECS

i.MX   6SoloLite Linux Multimedia Codecs Sources

5

L3.0.35_2.1.0_AACP_CODECS

i.MX   6SoloLite Linux AAC Plus Codec

6

L3.0.35_2.1.0_DEMO_IMAGE

i.MX   6SoloLite Linux Binary Demo Files

·         Target HW boards

o   i.MX6SL-EVK

·         New features

o   Updated thermal equation for i.MX 6SoloLite

o   Added Fuse check for all the devices

o   Enabled DISPLAY power gating feature on TO1.2

·         Known issues

o   For known issues and limitations please consult the release notes.

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

947件の閲覧回数
brucesun
Contributor III

I can't download L3.0.35_2.1.0_DEMO_IMAGE

0 件の賞賛
返信

947件の閲覧回数
EnriqueOchoaVaz
Contributor V

The release is no longer available because it was replaced by a newer release, please use the L3.0.35_4.1.0, you can get it using the links in this community doc.

i.MX 6 Q/D/DL/S L3.0.35_4.1.0 GA release

0 件の賞賛
返信