i.MX 6 DL/S L3.0.35_3.0.0 GA release

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6 DL/S L3.0.35_3.0.0 GA release

2,762 Views
EnriqueOchoaVaz
Contributor V

Hi All,

The new  i.MX 6 DL/S L3.0.35_3.0.0 GA release is now available on the http://www.freescale.com/site.

·         Files available

#

Name

Description

Files

1

L3.0.35_3.0.0_LINUX_DOCS

i.MX   6DualLite and i.MX 6Solo Linux GA BSP Documentation. Includes Release Notes,   Reference Manual, User guide. API Documentation

Link

2

L3.0.35_3.0.0_LINUX_MMDOCS

i.MX 6DualLite and i.MX 6Solo Linux GA Multimedia   Codecs Documentation. Includes   CODECs Release Notes and User's Guide

Link

3

L3.0.35_3.0.0_ER_SOURCE

i.MX   6DualLite and i.MX 6Solo Linux GA BSP Source Code Files

Link

4

L3.0.35_3.0.0_MM_CODECS

i.MX   6DualLite and i.MX 6Solo Linux GA Multimedia Codecs Sources

Link

5

L3.0.35_3.0.0_AACP_CODECS

i.MX   6DualLite and i.MX 6Solo Linux GA AAC Plus Codec

Link

6

IMX_6DL_6S_MFG_TOOL

Tool   and documentation for downloading OS images to the i.MX 6DualLite and   i.MX6Solo.

Link

7

L3.0.35_3.0.0_DEMO_IMAGE

i.MX 6DualLite and i.MX 6Solo Linux GA Binary Demo   Files.

Link

8

I.MX_6DL_S_VIVANTE_VDK_TOOLS

Set   of applications for the Linux L3.0.35_3.0.0 BSP, designed to be used by   graphics application developers to rapidly develop and port graphics   applications. Includes applications, GPU Driver with vprofiler enabled and   documentation.

Link

·         Target HW boards

o   i.MX 6DualLite SABRE-SDP

o   i.MX 6Solo SABRE-AI

o   i.MX 6DL SABRE-AI

·         New features

o   Support SabreSD RevC board

o   Support SabreAI RevC board

o   Upgrade GPU to 4.6.9-p8 version

o   Integrate VPU firmware 2.1.8_r34588

o   GPU performance tuning with AXI bus cache attribute enabled

·         Known issues

o   For known issues and limitations please consult the release notes.

Labels (2)
Tags (1)
4 Replies

1,417 Views
kimlim
Contributor III

Thanks for the link to download the latest BSP. However, I afraid the link is broken?

Service Temporarily Unavailable

The server is temporarily unable to service your request due to maintenance downtime or capacity problems. Please try again later.

0 Kudos
Reply

1,417 Views
EnriqueOchoaVaz
Contributor V

Hi Kim,

Can you try again to download the file again? I just checked and on my side is working correctly, if you still have the problem will be a regional problem with server providing the files to you. If you still have the problem can tell me where are you located?

1,417 Views
kimlim
Contributor III

is there any ubuntu rootfs support for this GA release? I saw an ubuntu image support for "i.MX 6 Q/D L3.0.35_1.1.0 GA release" but both the download link and community discussion are broken.

https://community.freescale.com/message/430478?et=watches.email.thread#430478

Unauthorized


Access to this place or content is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here.

0 Kudos
Reply

1,417 Views
EnriqueOchoaVaz
Contributor V

HI Kim,


We have an Ubuntu rootfs on the latest Linux BSP release provided by Freescale, please use the links on this community document.

i.MX 6 Q/D/DL/S L3.0.35_4.1.0 GA release

0 Kudos
Reply