hwcomposer_viv.imx6 library in android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hwcomposer_viv.imx6 library in android

1,087 Views
ali_sarlak
Contributor III

Dear NXP,

I know that "hwcomposer_viv.imx6.so" is for hardware compositor (GC320) library in android.

  • What's the equivalent library that do the same job in Linux (L3.0.35)?

Which API should I use in Linux:

  • i.MX_6_2D_API
  • i.MX_6_G2D_API
  • i.MX_6_Series_Wayland_Weston_User_Guide
  • Directfb1.4

according to "L3.0.35_4.1.0_docs"?

Yours,

0 Kudos
Reply
1 Reply

912 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ali

1. seems this is gpu driver, description can be found in

Graphics Processing Unit (GPU) Chapter of Linux Manual included in L3.0.35 documentation

http://www.nxp.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

2. proprietary gpu libs are provided as binaries only, one can try to get

sources using local marketing office.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply