hwclock --systohc command make freezing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hwclock --systohc command make freezing

1,254 Views
호영노
Contributor II

Hello,


I'm using the i.MX6 DL. 

When I first time test the custom board, 

I can set the system time and sync with hwclock by hwclock --systohc.

But after changed some of H/W peripherals,and making a new custom board, 

hwclock command is not working.

first, I set the system time by 

#date "2018-08-13 13:33:11" 
Then I can check the changed system time.

But for the saving to rtc, input the below message, 

# hwclock --systohc 

Then nothing changed and there is no reaction. 

It looks there is no response so it just wait some response.. 

Because kernel & rootfs is not changed but only my custom board's some part was changed,

So I thinking that some part making this problem.

Do you have any idea of this?? 

What can making this problem?

Labels (2)
0 Kudos
Reply
1 Reply

1,051 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

Previous test might work.

https://community.nxp.com/thread/436479 

Regards

0 Kudos
Reply