hub 1-1:1.0: unable to enumerate USB device on port -blog archive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hub 1-1:1.0: unable to enumerate USB device on port -blog archive

2,935 Views
Swamy
Contributor III

Hi All,

I am facing a problem. If I connect the USB device to my system, I am getting following error message.

hub 1-1:1.0: unable to enumerate USB device on port

I am using kernel-2.6.31 and also I have enabled HID Devices under DeviceDriver package..still this issue.

Please suggest

Regards,

Swamy

Tags (1)
0 Kudos
Reply
3 Replies

2,054 Views
harald_krapfenb
Contributor III

Such problems are mostly related to the hardware. Is this the internal root hub or an external? Check power and proper routing to the device I would suggest. Also turn on debugging, then you see a more detailed error message.

Regards, Harald

0 Kudos
Reply

2,054 Views
rohith1z
Contributor III

Hi,

I'm getting a same error on a custom board based on imx253.

The error is a timeout error.

Also get "devpath 1 ep0in 3strikes" when debugging is turned on.


Same port works fine in device mode.

Any pointers to debugging would be nice.


Thanks.

0 Kudos
Reply

2,054 Views
rohith1z
Contributor III

Issue I'm getting was traced to hardware and it's been fixed.

0 Kudos
Reply