how to write WKS file for rauc in imx8mq maaxboard? what is the default wks file for imx8mq ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to write WKS file for rauc in imx8mq maaxboard? what is the default wks file for imx8mq ?

3,955 Views
gonewithwind-peter
Senior Contributor I

Hi all,

I am playing rauc  to update my rootfs on imx8mq maaxboard,

I need an additional rootfs im image to burn SD card. but I do not know how to write the .wks file.

 Do you know where is the default wks file for imx8mq ? so I can add an additional partition  to write the additional rootfs. I  can not find it in the yocto  source code 

I can build my rauc in my yocto.

Thank you very much.

I have found someone mention the wks file at here, but it shows the wks not work .

https://community.nxp.com/t5/i-MX-Processors/Bitbake-after-add-RAUC-not-work-IMX8MN/m-p/1309665

I need the optee function ,so my uboot is SPL (I think, so I think I can not directly use it)

therefore, I want to know where is the default default wks file for imx8mq? I can modify it if I know

 

0 Kudos
Reply
12 Replies

3,931 Views
gonewithwind-peter
Senior Contributor I

I  add the IMAGE_FSTYPES = "tar.bz2 ext4 wic.gz wic.bz2 wic.map sdcard.bz2" in "imx/meta-sdk/conf/distro/include/fsl-imx-base.inc"  I get the similar  error  to here (someone posted : https://community.nxp.com/t5/i-MX-Processors/Error-when-building-Yocto-Sumo-with-Bitbake/m-p/879773  No IMAGE_CMD   

 

/home/yocto/yocto/source/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/dynamic-layers/qt5-layer/recipes-fsl/images/fsl-image-qt5.bb: No IMAGE_CMD defined for IMAGE_FSTYPES entry 'wic.map' - possibly invalid type name or missing support class
ERROR: /home/yocto/yocto/source/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/dynamic-layers/qt5-layer/recipes-fsl/images/fsl-image-qt5-validation-imx.bb: No IMAGE_CMD defined for IMAGE_FSTYPES entry 'wic.map' - possibly invalid type name or missing support class
ERROR: /home/yocto/yocto/source/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-validation-imx.bb: No IMAGE_CMD defined for IMAGE_FSTYPES entry 'wic.map' - possibly invalid type name or missing support class
ERROR: /home/yocto/yocto/source/imx-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-gui.bb: No IMAGE_CMD defined for IMAGE_FSTYPES entry 'wic.map' - possibly invalid type name or missing support class

 

I am using  yocto sumo, L4.14.98-2.0.0_ga

0 Kudos
Reply

3,947 Views
gonewithwind-peter
Senior Contributor I

Hi all.

I modified file ./imx-yocto-bsp/sources/meta-freescale/wicimx-uboot-spl-bootpart.wks  as below in  yocto sumo source code, can add WKS_FILE="imx-uboot-spl-bootpart.wks"  in local.conf.

but  after bitbake fsl-image-validation-imx to build the image , there is no additional rootfs partition in sdcard.

it seems the bitbake do not use the file: WKS_FILE="imx-uboot-spl-bootpart.wks". because I put a wrong file name (eg:imx-uboot-spl-bootpart.wks.in), bitbake still can build, no error to show that the file imx-uboot-spl-bootpart.wks.in is not found).

any help? how can I add or modify the WKS file?

 

Thank you.

0 Kudos
Reply

3,942 Views
jimmychan
NXP TechSupport
NXP TechSupport

Please read the Chapter 4.5.13 "How to build imx-boot image by using imx-mkimage" in the i.MX Linux User’s Guide​

0 Kudos
Reply

3,939 Views
gonewithwind-peter
Senior Contributor I

@jimmychan 

Thank you very much.

 I have read the doc you posted. it's useful for me. but  it's for only linux guide. not the yocto guide .

I am using the yocto L4.14.98-2.0.0_ga . after build, it will generate rootfs.sdcard.bz2. image.

I think I need to generate rootfs.wic.bz2 code so that the bitbake can use wks file. 

now if it generates rootfs.sdcard.bz2, the yocto bitbake can not enable wks function and can not read the wks file , right?

0 Kudos
Reply

3,928 Views
jimmychan
NXP TechSupport
NXP TechSupport

In the newer version of BSP (e.g. L5.4.24_2.1.0), there is .wic file under the "tmp/deploy/images" folder after the building. Please try to use the newer version of BSP.

0 Kudos
Reply

3,915 Views
gonewithwind-peter
Senior Contributor I

hi @jimmychan 

and all,

 

Thank you very much for you reply so soon.

firstly, I can not change newer version, I have to use  L4.14.98-2.0.0_ga . because our colleagues node code can not work well in newer version. there are a lots work to do. 

yes ,I found the files are in the folder imx-yocto-bsp/build-xwayland/tmp/deploy/images/imx8mqevk/

but I am not sure what exactly files will be written in to Sd card. especially  what is the u-boot files  will be written in to Sd card?

let me describe more  detail about my situations:

I need rauc , so I need .wks file to add additional roofts  . so  I  add the following file in local  config file:

 

WKS_FILE="imx-uboot-spl-bootpart.wks"
IMAGE_BOOT_FILES = "imx8mq_m4_TCM_hello_world.bin imx8mq_m4_TCM_rpmsg_lite_pingpong_rtos_linux_remote.bin imx8mq_m4_TCM_rpmsg_lite_str_echo_rtos.bin em-sbc-imx8m.dtb Image"
IMAGE_FSTYPES_append = " wic"
UBOOT_CONFIG_append = " wic"
SOC_DEFAULT_IMAGE_FSTYPES_append = " wic"

 

--

after that: it can build rootfs.wic.bz2 image with an additional rootfs  to burn SD card (not the default rootfs.sdcard.bz2) and it can read *wic while building.

as I mentioned before ,I used optee, so I not sure sure I will use which .wks file ,

 there are two wks files at     meta-freescale/wic/imx-uboot-spl-bootpart.wks 

# The disk layout used is:
# - ----- --------- -------------- --------------
# | | SPL | u-boot | boot | rootfs |
# - ----- --------- -------------- --------------
# ^ ^ ^ ^ ^
# | | | | |
# 0 1kiB 69kiB 4MiB 16MiB + rootfs + IMAGE_EXTRA_SPACE (default 10MiB)
#
part SPL --source rawcopy --sourceparams="file=u-boot-spl.bin" --ondisk mmcblk --no-table --align 1
part u-boot --source rawcopy --sourceparams="file=imx-boot-imx8mqevk-sd.bin-flash_ddr4_em" --ondisk mmcblk --no-table --align 69
part /boot --source bootimg-partition --ondisk mmcblk --fstype=vfat --label boot --active --align 4096 --size 16
part / --source rootfs --ondisk mmcblk --fstype=ext4 --label root_A --align 4096 --overhead-factor 1
part / --source rootfs --ondisk mmcblk --fstype=ext4 --label root_B --align 4096 --overhead-factor 1

bootloader --ptable msdos

 

and file:

  imx-uboot-spl-bootpart.wks 

 

# The disk layout used is:
# - --------- -------------- --------------
# | | u-boot | boot | rootfs |
# - --------- -------------- --------------
# ^ ^ ^ ^
# | | | |
# 0 1kiB 4MiB 16MiB + rootfs + IMAGE_EXTRA_SPACE (default 10MiB)
#
part u-boot --source rawcopy --sourceparams="imx-boot-imx8mqevk-sd.bin-flash_ddr4_em" --ondisk mmcblk --no-table --align 1
part /boot --source bootimg-partition --ondisk mmcblk --fstype=vfat --label boot --active --align 4096 --size 16
part / --source rootfs --ondisk mmcblk --fstype=ext4 --label root_A --align 4096
part / --source rootfs --ondisk mmcblk --fstype=ext4 --label root_B --align 4096

bootloader --ptable msdos

 

----

so my qestions are:

1. at line :bootloader --ptable msdos    . the bootloader is msdos will be written into SD card? right? I do not need to modify it?

2. part /boot     will read "IMAGE_BOOT_FILES = xxxx"  in local.conf. I write the files name there. after burning sdcard. the files are boot partition that are same as rootfs.scard,bz2. I think it correct. it includes Kernel image, dtb ...

 

3. the most important Qz: what is the u-boot file ?. I read your   kernal guide. it should be flash.bin, in the  folder tmp/deploy/images/imx8mqevk/, there is no flash.bin. it seems changes name to imx-boot-imx8mqevk-sd.bin-flash_ddr4_em ? (I find they are  same size, because I added maaxboard in imx8mqevk-  and changed imx8mqevk.conf  line :#IMXBOOT_TARGETS = "flash_evk flash_evk_no_hdmi flash_dp_evk"
IMXBOOT_TARGETS = "flash_ddr4_em"  ), so it seems it's the correct u-boot file  that finally be written into sdcard? right?

tmp/deploy/images/imx8mqevk$ ls imx-boot* -l
 imx-boot-imx8mqevk-sd.bin -> imx-boot-imx8mqevk-sd.bin-flash_ddr4_em
 imx-boot-imx8mqevk-sd.bin-flash_ddr4_em

....

 

 

3. if I use imx-uboot-spl-bootpart.wks , so I need to add u-boot-spl.bin ? right?

or imx-boot-imx8mqevk-sd.bin-flash_ddr4_em always includes u-boot-spl.bin?  and DO NOT need  u-boot-spl.bin? I am not clear. it seems imx-boot-imx8mqevk-sd.bin-flash_ddr4_em always includes u-boot-spl.bin from the kernal guide and mkimage in yocto?

 

Thank you very much.

 

 

 

 

 

0 Kudos
Reply

3,910 Views
gonewithwind-peter
Senior Contributor I

hi all

I can not boot the board with both imx-uboot-spl-bootpart.wks  and imx-uboot-bootpart.wks 

I think my sdcard file structure(partition) is wrong. or the u-boot file is not correct.

any help?

Tags (1)
0 Kudos
Reply

3,902 Views
gonewithwind-peter
Senior Contributor I

hi

@jimmychan 

I make sure th u-boot image is imx-boot-imx8mqevk-sd.bin-flash_ddr4_em

(I tested in rootfs.sdcard.bz2,if I remove this file imx-boot-imx8mqevk-sd.bin-flash_ddr4_em ->imx-boot-imx8mqevk-sd.bin, can not build   rootfs.sdcard.bz2 successfully, it shows can not find imx-boot-imx8mqevk-sd.bin) ,so my u-boot file is correct!

but why I use wks to build rootfs.wic.bz2 image. it can not boot up the board?

so the below line in wks is wrong :

part u-boot --source rawcopy --sourceparams="imx-boot-imx8mqevk-sd.bin-flash_ddr4_em" --ondisk mmcblk --no-table --align 1

 

do I need to change to align 0?

 

 

let me try.

 

any help?

Thank you

0 Kudos
Reply

3,884 Views
gonewithwind-peter
Senior Contributor I

Hi @jimmychan 

and all 

I read the kernel guide , how to write u-boot to SD card,

the command is 

sudo dd if=imx-boot-imx8mqevk-sd.bin-flash_ddr4_em  of=/dev/sdb bs=1k seek=33 conv=fsync

there is 33 for option seek,  does it mean the data will write on the sd card from 33 *1024(33K) not from postion 0 ,right?

it works. when I use the command line.

so do I need change the wks file  align to 33 ? right?

part u-boot --source rawcopy --sourceparams="imx-boot-imx8mqevk-sd.bin-flash_ddr4_em" --ondisk mmcblk --no-table --align 33      # not default 1    ??????

let me try.

 

any help?

0 Kudos
Reply

3,882 Views
gonewithwind-peter
Senior Contributor I

hi @jimmychan 

and all 

finally, my u-boot code works!

 

need change  align to 33  in wks file as below:

part u-boot --source rawcopy --sourceparams="imx-boot-imx8mqevk-sd.bin-flash_ddr4_em" --ondisk mmcblk --no-table --align 33

finished the first setp for rauc

Thank you

 

Tags (1)
0 Kudos
Reply

3,874 Views
jimmychan
NXP TechSupport
NXP TechSupport
Very nice.
0 Kudos
Reply

3,854 Views
gonewithwind-peter
Senior Contributor I

hi

@jimmychan 

 

I have more question about rauc  and  u-boot-fw-utils(fw_printenv, fw_setenv), I post  here

https://community.nxp.com/t5/i-MX-Processors/I-can-not-build-u-boot-fw-utils-in-yocto-for-maaxboard-...

please have a look.

Thank you.

 

0 Kudos
Reply