how to use the I2C_INT in imx28_evk?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to use the I2C_INT in imx28_evk?

1,424 次查看
meifang
Contributor I

In imx28_EVK sch file,the touch screen use a interrupt of the pin I2C_INT.

I can't understand how to work of it. There is no input signal by this pin.

0 项奖励
回复
3 回复数

1,330 次查看
igorpadykov
NXP Employee
NXP Employee

Hi fang

this signal is not used, it is for optional

LCD touch controller. You can check LCD schematic,

SPF-26139_revB.pdf, JP2 - DNP

MX28_LCD_DESIGN_FILES : i.MX28 LCD Design Files

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,330 次查看
meifang
Contributor I

Hi chip

thanks very much for your answer so quickly.

If this pin is optional for LCD touch control,how control the interrupt of touch screen?

I used L2.6.35_1.1.0 and tslib-1.0,but the touch not work right.

0 项奖励
回复

1,330 次查看
igorpadykov
NXP Employee
NXP Employee

Hi fang

in L2.6.35_1.1.0 pin I2C_INT is not used.

Best regards

chip

0 项奖励
回复