The mx6ull evk board use rmii 50MHz clk from MAC to phy. But in our hardware design use rmii with 50MHz clk from phy. i change u-boot/board/freescale/mx6ullevk/mx6ullevk.c
eg. FEC1(ENET2).
static iomux_v3_cfg_t const fec2_pads[] = {
MX6_PAD_GPIO1_IO06__ENET2_MDIO | MUX_PAD_CTRL(MDIO_PAD_CTRL),
MX6_PAD_GPIO1_IO07__ENET2_MDC | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET2_TX_DATA0__ENET2_TDATA00 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET2_TX_DATA1__ENET2_TDATA01 | MUX_PAD_CTRL(ENET_PAD_CTRL),
-MX6_PAD_ENET2_TX_CLK__ENET2_REF_CLK2 | MUX_PAD_CTRL(ENET_CLK_PAD_CTRL),
+MX6_PAD_ENET2_TX_CLK__ENET2_TX_CLK | MUX_PAD_CTRL(ENET_CLK_PAD_CTRL),
MX6_PAD_ENET2_TX_EN__ENET2_TX_EN | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET2_RX_DATA0__ENET2_RDATA00 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET2_RX_DATA1__ENET2_RDATA01 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET2_RX_EN__ENET2_RX_EN | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET2_RX_ER__ENET2_RX_ER | MUX_PAD_CTRL(ENET_PAD_CTRL),
};
and
static int setup_fec(int fec_id)
{
struct iomuxc *const iomuxc_regs = (struct iomuxc *)IOMUXC_BASE_ADDR;
int ret;
if (fec_id == 0) {
....
} else {
/*
* Use 50M anatop loopback REF_CLK2 for ENET2,
* clear gpr1[14], set gpr1[18].
*/
- clrsetbits_le32(&iomuxc_regs->gpr[1], IOMUX_GPR1_FEC2_MASK,
- IOMUX_GPR1_FEC2_CLOCK_MUX1_SEL_MASK);
-
+ /* clk from phy, set gpr1[14], clear gpr1[18] */
+ clrsetbits_le32(&iomuxc_regs->gpr[1], IOMUX_GPR1_FEC2_MASK,
+ IOMUX_GPR1_FEC2_CLOCK_MUX2_SEL_MASK);
}
...
}
But i can't make FEC1 work in u-boot.
May i miss something?