how to use ov 5642

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to use ov 5642

1,904 次查看
marshall123
Contributor II

Dear community:

hello, i have an ov5642 module using parallel connector ,one i.mx6qp sabre SD board and an environment running yocto project. how can i use this module on board? should i change the kernel or just type commands in board command line or write my code and cross compile it then run on the board?

Do you have a guide or some documents? sorry for the stupid question but I really donno how to continue.

thank you!

0 项奖励
回复
1 回复

1,709 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

please check sect.19.2 OV5642 Using parallel interface attached Linux Manual

and useful links
https://community.nxp.com/thread/329673
https://boundarydevices.com/ov5642-auto-focus-on-i-mx6/

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复