how to use mfg tools

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to use mfg tools

1,336 次查看
chewhouming
Contributor III

in DOS, in Sb_loader folder, i run

sb_loader.exe -f u-boot-mx6q-sabrelite.bin

it reply waiting for HID device for 2 seconds

I brick my sabrelite board, try using mfg tools but without successful.

i tried following link http://comments.gmane.org/gmane.linux.linaro.devel/11942

Choose Options->Configuration...->USB-Ports

  and search for something like "Linux-File-Stor..." or "HID-device..."

There is no something like "Linux-File-Stor..." or "HID-device..."

1 回复

1,181 次查看
igorpadykov
NXP Employee
NXP Employee

Hi chew

you can test if USB interface is healthy with SDK

(one can run tests with jtag)

i.MX 6Series Platform SDK

or probably just replace processor.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------