how to use ldb/lvds in android8 of imx8mq ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to use ldb/lvds in android8 of imx8mq ?

35,388 Views
jiangyaqiang
Contributor V

Hi  anyone:

   Is there any document about how to use lvds in android8 of imx8mq platform ?

Best Regards.

25 Replies

28,749 Views
lswdneil
Contributor I

Hi, Jiang:

    Thank you for  your  sn65dsi84 's  code . I have used it and the  LCD(1920X1080) can  show .   but  met some questions, please see the attched file, 1.) the screen shift to right  2.) the colors have distortion.

977a6b34c9f62704843c3631aa107ba.jpg

  Can you give me some advice?   

thanks.

13534273512

Thomas He.

0 Kudos
Reply

28,749 Views
hankwang
Contributor V

Hi Dong,

               Do you have resolved this issue? I have the same issue.

0 Kudos
Reply

28,749 Views
hankwang
Contributor V

  The issue fixed.  The dsi parameters must be modified as below :

   The dsi->mode_flags = MIPI_DSI_MODE_VIDEO | MIPI_DSI_CLOCK_NON_CONTINUOUS.

0 Kudos
Reply

25,826 Views
shraddha
Contributor I

where to find dsi and change this in mode_flags = MIPI_DSI_MODE_VIDEO | MIPI_DSI_CLOCK_NON_CONTINUOUS?
@hankwang 

0 Kudos
Reply

28,735 Views
jiangyaqiang
Contributor V

HI:

does you use external clock or dsi clock for sn65dsi clock input ?

江亚强

软件工程师

Shenzhen Huameishi Technology Co., Ltd

深圳市华美视科技有限公司

深圳市南山区科苑路6号科技园工业大厦605

Tel:0755-26037882-616

Mail:yaqiang.jiang@huameishi.com

0 Kudos
Reply

28,714 Views
hankwang
Contributor V

HI,  i use dsi clock. My pixel clock is 72Mhz. So i set 432Mhz and Divisor is 6.

0 Kudos
Reply

28,714 Views
jiangyaqiang
Contributor V

HI  Hank wang:

          Thanks.

          but in sn65dsi84 datasheet , when use dsi clock as input , the dsi clock must be set as continuous. 

           BTW: have you try other  lcd resolution ?

datasheet:

8.3.1 Clock Configurations and Multipliers
The LVDS clock may be derived from the DSI channel A clock, or from an external reference clock source. When
the MIPI D-PHY channel A HS clock is used as the LVDS clock source, the D-PHY clock lane must operate in
HS free-running (continuous) mode; this feature eliminates the requirement for an external reference clock
reducing system costs

0 Kudos
Reply

28,714 Views
hankwang
Contributor V

Hi , I only tested 1920*1080 resolution. But I also have the same issue in another panel (1280*720).But i did not to test. 

Maybe i will test in few days. 

0 Kudos
Reply

28,749 Views
leemeiyung
Contributor I

HI Jiang:

   Follow your offered sn65dsi85 driver, I can dispaly 800x600@60Hz while use sn65dsi84 for mipi conver lvds, but encounter an "no singal" tips on another LCD with 1920x1080 resolution, when set CCSR 0x3c as 0x10, I can got the test pattern,  could you remind me what's wrong in the process。

BTW,use the same dts and kernel, I do the blowing test:

1) test pattern with single lvds chanel mode  on a 800x600 lcd -- ok

2) mipidsi show image to lvds single lvds chanel mode  on 800x600 lcd -ok

3) test pattern with dual lvds chanel mode on a 1920x1080 lcd -- ok

4) test pattern witch dual lvds chanel mode (forced in 800x600@60hz) on the 1920x1080 lcd -ok

5) mipi dsi show image to lvds with dual lvds chanel mode (forced in 800x600@60hz) fail, but while connect the 800x600 resolution lcd in one lvds channel, i got the image.

Thanks.

0 Kudos
Reply

28,749 Views
oliverkuo
Contributor IV

Hi Frank,

I'm also trying to enable sn65dsi84 on our custom board, we use a 1024*600 LVDS panel.

However, the DSI driver can't work out the CM/CN/CO values for D-PHY ref_clk.

Could you share your dts file and timing table of the panel?

imx_nwl_try_phy_speed (583): bit_clk = 403200000 ; pixclock = 50400000

nwl_dsi-imx mipi_dsi@30A00000: [drm:imx_nwl_try_phy_speed] *ERROR* Cannot setup PHY for mode: 1024x600 @50400 kHz

nwl_dsi-imx mipi_dsi@30A00000: [drm:imx_nwl_try_phy_speed] *ERROR* PHY_REF clk: 27000000, bit clk: 403200000

Thanks a lot.

0 Kudos
Reply

28,749 Views
jiangyaqiang
Contributor V

HI :

you can turn up the frequency.

For 1024*600 LVDS, I success in kernel 4.9 but fail in 4.14.

江亚强

软件工程师

Shenzhen Huameishi Technology Co., Ltd

深圳市华美视科技有限公司

深圳市南山区科苑路6号科技园工业大厦605

Tel:0755-26037882-616

Mail:yaqiang.jiang@huameishi.com

28,749 Views
merlinthewizard
Contributor I

Hi Jiang,

I'm trying to add sn65dsi84 to my kernel but I have some trouble with device tree, it is possible to have your entire dts? I'm not very skilled in this stuff yet and I guess I'm making mny errors.

Let me know,

Thanks

0 Kudos
Reply

28,733 Views
jiangyaqiang
Contributor V

HI merilin:

It's the same with fsl-imx8mq-evk-dcss-rm67191.dtsi except:

江亚强

软件工程师

Shenzhen Huameishi Technology Co., Ltd

深圳市华美视科技有限公司

深圳市南山区科苑路6号科技园工业大厦605

Tel:0755-26037882-616

Mail:yaqiang.jiang@huameishi.com

28,733 Views
oliverkuo
Contributor IV

Hi,

Thanks for your reply.

I found the algorithm of computing CM/CN/CO was revised in Linux version(4.14.98), I think this issue will be fixed on next release.

0 Kudos
Reply

28,733 Views
jiangyaqiang
Contributor V

HI Lee:

Most likely it's the display_timing problem.

江亚强

软件工程师

Shenzhen Huameishi Technology Co., Ltd

深圳市华美视科技有限公司

深圳市南山区科苑路6号科技园工业大厦605

Tel:0755-26037882-616

Mail:yaqiang.jiang@huameishi.com

0 Kudos
Reply

28,733 Views
念祖姚
Contributor II

Hi Jiang:

      Thanks for  your  share!    I added  the panel-sn65dsix.c and  panel-dsi85.h   into   my ststem,  and I  encountered such a problem,the  dmesg  indicated that  

the mipi_dsi_bridge  can't   find  the  i2c  client  device  sn65dsi8x.

      I added some  log massages and then i  find  that  the  sn65dsi8x  client_dev->dev.driver  = NULL.    Is  the  sn65dsi8x  need  a   i2c  device driver?,   Have you encountered this  problem?

   My  kernel  log:

   [ 1.052093] [drm] Initialized
   [ 1.061372] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
   [ 1.068015] [drm] No driver support for vblank timestamp query.
   [ 1.074129] imx-drm display-subsystem: bound imx-dcss-crtc.0 (ops dcss_crtc_ops)
   [ 1.081637] nwl_dsi-imx mipi_dsi@30A00000: Using DCSS as input source
   [ 1.088478] panel-ti-sn65dsi8x 30a00000.mipi_dsi_bridge.0: failed to find client platform device
   [ 1.097285] panel-ti-sn65dsi8x 30a00000.mipi_dsi_bridge.0: Yao-log:client_dev->dev.driver == NULL!!!
   [ 1.106541] nwl-mipi-dsi 30a00000.mipi_dsi_bridge: [drm:nwl_dsi_host_attach] lanes=4, format=0x0 flags=0x813
   [ 1.116450] imx-drm display-subsystem: bound mipi_dsi@30A00000 (ops imx_nwl_dsi_component_ops)
   [ 1.129560] [drm] OPIPE_CFG: gamut = 3, nl = 1, pr = 1, pix_format = 875713089
   [ 1.655077] function:sn65_panel_enable line:1044 -----------
   [ 1.721128] Console: switching to colour frame buffer device 240x67
   [ 1.783389] imx-drm display-subsystem: fb0: frame buffer device

Thanks & Best Regards

  姚念祖 
 Address: 武汉市洪山区光谷大道特一号国际企业中心
0 Kudos
Reply

28,733 Views
jiangyaqiang
Contributor V

Hi:

It just a simple driver provided i2c client for panel-sn65dsi.c.

江亚强

软件工程师

Shenzhen Huameishi Technology Co., Ltd

深圳市华美视科技有限公司

深圳市南山区科苑路6号科技园工业大厦605

Tel:0755-26037882-616

Mail:yaqiang.jiang@huameishi.com

0 Kudos
Reply

28,733 Views
venkatesh_selva
Contributor II

Hi Jiang,

Thanks for the reply. In my case I'm using SN65DSI84 as bridge and auo t21hvn01 for panel. Can you share your changes in fsl-imx8mq-com.dts & fsl-imx8mq-com.dtsi files?

Can I ask you what panel you have used? If the panel is not similar, I guess I need to write drm brdge driver for panel-simple.c

In my so far combinations I couldn't see DSI clock.

Venkatesh

0 Kudos
Reply

28,733 Views
jiangyaqiang
Contributor V

HI :

As attachment.

Hope it can help for you.

BTW, some clock doesn't support by imx8mq, you can higher it up a little.

江亚强

软件工程师

Shenzhen Huameishi Technology Co., Ltd

深圳市华美视科技有限公司

深圳市南山区科苑路6号科技园工业大厦605

Tel:0755-26037882-616

Mail:yaqiang.jiang@huameishi.com

28,733 Views
jiangyaqiang
Contributor V

sorry, I got it, it much convert MIPI to LVDS.