how to use flexCAN in imx6ull processor ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to use flexCAN in imx6ull processor ?

1,260件の閲覧回数
somnath_roy
Contributor I

hi all,

    i am using a SOM module by toradex it came with imx6ull processor 

i have changed the dtsi file and my module is loaded in startup. 

but i am getting a msg as 

[   13.641388] CAN device driver interface
[  OK  ] Reached target System Initialization.
[   13.677653] 2094000.can supply xceiver not found, using dummy regulator

and when i am using cansend utility i am not getting and signal in CAN_tx pin.

yet i am using can xceiver IC UJA1161 and my xceiver is powered up.

ラベル(2)
0 件の賞賛
返信
1 返信

1,102件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Somnath

please connect other board or protocal analyzer and for testing

one can use unit tets (folder ..test/can) :
imx-test
www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-test-5.7.tar.gz

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信