Hello,
To use full trace abilities of ARM core it is needed to configure the ETM,
corresponding ETM (trace) pins of the I.MX6UL, and special trace hardware
(Dstream / DS-5). Mainly it is recommended to use the ETB. In this mode
you don't need to configure ETM, IO pins and you don't need even special
trace hardware. The trace is collected via JTAG. The disadvantage in this mode
is that the trace is not collected in real time and the maximal size of trace is 4K.
Perhaps it makes sense to apply to ARM directly regarding the DSTREAM.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------