how to support usb gadget serial function correctly for imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to support usb gadget serial function correctly for imx6q

2,540 Views
huiwang
Contributor II

system:android 5.1

platform:imx6q

now I do such operations below to add usb acm function:

1.add some code in init.freescale.usb.rc

   on property:sys.usb.config=acm,adb
   write /sys/class/android_usb/android0/enable 0
   write /sys/class/android_usb/android0/idVendor 18d1
   write /sys/class/android_usb/android0/idProduct 4e45
   write /sys/class/android_usb/android0/f_acm/instances 1
   write /sys/class/android_usb/android0/functions ${sys.usb.config}
   write /sys/class/android_usb/android0/enable 1
   start adbd
   setprop sys.usb.state ${sys.usb.config}

2.adb shell to set the usb property

   #setprop persist.sys.usb.config acm,adb    the default property is mtp,adb

3.install the gadget driver on my windows computer, it can identify the serial of COM24, and I can also communicate using this COM

But now question is when i want to change the usb property back 

    #setprop persist.sys.usb.config mtp,adb

the android system will reboot at once, and the property is also acm,adb

what wrong with it and how can i config correctly to support usb gadget serial (acm) function?

Thanks a lot !

Labels (1)
Tags (4)
0 Kudos
Reply
2 Replies

2,276 Views
huiwang
Contributor II

add some more information:

revise the default usb prop (mtp,adb) to (ptp,adb) ,  and change it back to(mtp,adb). The android system is running OK without rebooting.

0 Kudos
Reply

2,276 Views
jimmychan
NXP TechSupport
NXP TechSupport
0 Kudos
Reply