how to support SN65DSI84 to imx8mm in Android OS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to support SN65DSI84 to imx8mm in Android OS

1,181 Views
Ruban1
Contributor II

how to support SN65DSI84 to imx8m mini in Android OS. Or but by default as i insert the SN65DSI84 chip in MIPI will the LVDS display work. If required any drivers can you provide the drivers and path where i have to place and which image should i have to build  or should i rebuild everything after adding the drivers and then run to the Android OS throught SD card mode.

Labels (1)
0 Kudos
Reply
2 Replies

1,176 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ruban

 

as android based on linux one can look at SN65DSI84 linux support on

https://github.com/TechNexion-customization/linux-imx-tn/blob/tn-imx_4.14.98_2.0.0_ga-wip-mipi2lvds/...

 

Best regards
igor

0 Kudos
Reply

1,174 Views
Ruban1
Contributor II

Sorry for the mis guide the chip is SN65DSI83TPAPRQ1 . which you have sent is upgraded one. Can you kindly provide related documents for SN65DSI83TPAPRQ1.

0 Kudos
Reply